Part Number: TMS320F28075
Other Parts Discussed in Thread: C2000WARE
Tool/software:
We have custom boards with the said uC. We were testing total 5 prototype boards. We want to run the uC wiht 120MHz clock which is derived from PLL with INTOSC2 as clock source. This is selected based on TRM.
But when we tested, we observed that only 1-2 boards correctly lock the PLL. 1 board intermittently lock PLL and 2 boards doesn't lock at all.
However, when we switched PLL clock source to INTOSC1 all boards work correctly. PLL gets locked without fail.
We are using InitSysPll library function to enable the PLL.
Regards,
Akshay Dandekar