This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28P65X: Simultaneously read MCAN_A and CAN_A for LAUNCHXL-F28P65X

Part Number: LAUNCHXL-F28P65X

Tool/software:

Good evening!

I want to read data from the CAN_A and simultaneously from the MCAN_A bus of the TI F28P65 using simulink.
Is this in general possible? I was wondering as I thought these two busses run over the same CAN tranceiver, thus when transmitting data I would kind of crash.


With best regards,

Isabella Flor

  • Hi Isabella,

    DCAN and MCAN frames are not compatible on the same bus.  MCAN can interpret the DCAN frame but not the other way around.  MCAN frame has a different field assignment and DCAN node will report this as an error.

    Regards,

    Joseph