This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
david,
am using TMS320F2812 kit , am new to this .but now i want to do a project to generated pwm for sr motor., i have CCS 3.3(S.R.12) and xds100usb emulator. successfully i have connected thrugh those , but i want to do some simple programming in that, but i failed to loaad inon chip FLASH or on chip RAM. can you guide to complete my work......, please am expecting 100% result from you .
When using CCS3.3v,
Load program to RAM - File -> Load program (select the .out file to be programmed)
Load program to FLASH - Use CCS plugin and select the .out file to be programmed into flash.
Regards,
Manoj
hi manoj,
my problem was solved . simply i changed my device tms320f2812. then in new processor IC flash has worked.
Thanks