This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Programming F2812 using Flash memory.

Hello Friends,

I am working on F2812 microcontroller. I am trying to program using flash memory for stand alone operation. I have succeeded in flashing the program. But for some reason none of the interrupts seems to be working. I have three LED's to confirm the operation while the program is running. Two of them are in the main program. One is in the interrupts. 

While running the program in standalone, I am able to observe the two LEDs mentioned in the main program are working. But the LED which is controlled in the Interrupts is not working. Do i have to make any setting changes in the CCS V3.3.

Please help me with the problem.

Thanks and Regards. 

Hari Prasad. A