Part Number: LAUNCHXL-F28379D
Tool/software:
Hi everyone,
I am currently using the F28379D LaunchPad for a university Capstone project and would like to power it using an external supply (i.e. without the USB connection). I have been reading the provided User Guide to determine how this should be done and wanted to ask some questions to ensure my understanding is correct.
1) Does the LaunchPad require only +3.3 V externally to be powered in standalone mode, or does it require both +3.3V and +5 V? Reading through a similar post on E2E has lead me to believe that while the +3.3 V is required to power the LaunchPad, the +5 V power rail simply allows the user to route +5 V to a different device using the LaunchPad.
2) To supply +3.3 V externally to the LaunchPad, I would follow Configuration 2 from Table 1 of the User Guide. This voltage needs to be routed to header J10, which has 3 pins: 1 for +3.3 V, and 2 for GND. According to the schematic provided in the user guide, both ground pins are shorted together. Would it suffice to connect only 1 of the GND pins to the supply ground, or should both J10 GND pins be connected?
3) Suppose I have powered the LaunchPad with a +3.3 V external supply using J10. I now want to provide the LaunchPad with +5 V. To do this, it would be preferable to use Configuration 2 from Table 2 of the User Guide, where +5 V is provided through the on-board step-up regulator (which boosts the supplied +3.3 V to +5 V). In this configuration, can JP6 then be used to provide +5 V externally to a different device?
4) To reiterate, I am using Configuration 2 from Table 1 (to power the Launchpad with +3.3 V) and Configuration 2 from Table 2 (to supply +5 V to the LaunchPad as a means of powering other devices). I have observed that JP1, JP2, and JP3 should be left open using these configurations. In this case, is it required that I remove the jumpers from JP1, JP2, and JP3 if I am supplying the LaunchPad with an external +3.3 V? Generally, is there anything that needs to be done with jumpers JP1 through JP5 to ensure there are no issues when powering the LaunchPad without the USB connector?
Any confirmations would be greatly appreciated!