This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: Wow can I make my own PDO definitions?

Tool/software:

Hi Experts,

Customer is working with TI f28p65x launchpad and using ethercat communication with Beckhoff c603. The example for f28p65x_cpu1_dc_eepromemu_echoback is working:

Question is how can I make my own PDO definitions? In the example, the -> ethercat_subdevice_ssc_and_demo_setup.exe is given which created -> f28p65x_ssc_config.xml which is imported in the SSC tool to create the F28P65x CPU1 EtherCAT SubDevice.xml and C files.

Should I manually edit the f28p65x_ssc_config.xml and then import in the SSC tool (or) is there another way?

About this post from E2E:

As I understand the thread, I have to load the xml config in SSC tool and create a new excel sheet with my definitions and generate the files. Is this the right workflow? Additionally, how can I change the Distribution Clock Frequency?

Do I need to set it in the launchpad or the master Beckhoff PC?

Thank you.

Regards,

Archie A.