Part Number: TMS320F280037-Q1
Tool/software:
We are using PMIC from a different company, we are checking compatibility, can you please comment on the following?
For power up sequence:
If the slew rate is faster than the specified 8 mV/us, ESD protection can activate, can you please provide details on this protection (what happens to the uC)?.
If slew rate is slower than the specified 100mV/us, the only effect is XRSn toggling, which does not affect microcontroller, only will affect devices connected to XRSn, correct?
For power down sequence:
Are the same effects than power up? if not, can you please provide details for faster and slower than specified slew rate?
For Figure 6-9. Internal VREG Power Up Sequence, the right side (falling edges) represent what is going to happen when the power is going down, the monitors are released, then the micro pulls down reset, is this correct? can micro pull down reset without power? Is it only in some voltage range while the voltage goes to 0? do you have details?
Any other critical parameters to check compatibility?