Part Number: TMS320F28379D
Tool/software:
Hi,
I am using C2000 Microcontroller. I am using the simulink C2000 blockset. Currently I'm having this issue "Device is held in reset". Previously it works totally fine.
Here i share more about the error:
SEVERE: C28xx_CPU1: Trouble Writing Memory Block at 0x5fb00 on Page 0 of Length 0x2: (Error -1137 @ 0x6) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 12.7.0.00105) SEVERE: C28xx_CPU1: Error occurred during flash operation: Target failed to write 0x05FB00@Program
SEVERE: C28xx_CPU1: Trouble Writing Memory Block at 0x5f800 on Page 1 of Length 0x2: (Error -1137 @ 0x5F802) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 12.7.0.00105) SEVERE: C28xx_CPU1: Error occurred during flash operation: Target failed to write 0x0005F800@Data
SEVERE: C28xx_CPU1: Trouble Writing Memory Block at 0x5fb00 on Page 0 of Length 0x2: (Error -1137 @ 0x6) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 12.7.0.00105) SEVERE: C28xx_CPU1: Error occurred during flash operation: Target failed to write 0x05FB00@Program
SEVERE: C28xx_CPU1: Trouble Writing Memory Block at 0x5f800 on Page 1 of Length 0x2: (Error -1137 @ 0x5F802) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 12.7.0.00105)
SEVERE: C28xx_CPU1: Error occurred during flash operation: Target failed to write 0x0005F800@Data
SEVERE: C28xx_CPU1: Error initializing flash programming: Interface returned from dll, but flash is not available on this device.
SEVERE: C28xx_CPU2: Trouble Reading Register PC: (Error -1137 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 12.7.0.00105) SEVERE: C28xx_CPU2: Trouble Reading Register ST1: (Error -1137 @ 0x6) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 12.7.0.00105)