This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320LF2401A: TMS320F240PA

Tool/software:

hello,

i have the above controller, i need to backup the flash and write it on another one. i tried to read it with XDS510 usb Blackhawk, i got communication between the pc and tool but i can not got the flash using CCS 3.3 
in the setting before i run the studio is there a lot of option of controllers that xds510 blackhawk emulator supported. but for f24x there is no BHE near it. that mean i have to get a file with it the ccs know that it supported this controler
i hope some one understand me due to my language

it is very important , the customer have to get his device working, is there no device on the mark 
should i buy xds510 spectrum ? 
can any one help me to get GEL file or EVM for f240 from blackhawk ?

thanks