Part Number: LAUNCHXL-F28P65X
Other Parts Discussed in Thread: C2000WARE, SYSCONFIG
Tool/software:
I am trying to find a working example for how to use MCAN.
I have the LAUNCHXL-F28P65X board connected to a Komodo CAN DUO so i can see traffic.
The switch on the launchpad is set to use the onboard transceiver.
When I try the CAN examples in C2000Ware_5_05_00_00\driverlib\f28p65x\examples\c28x\can I can get the examples to work if I change the GPIO's to 4/5.
I tried the same thing with the MCAN examples in C2000Ware_5_05_00_00\driverlib\f28p65x\examples\c28x\mcan but that doesn't seem to be enough to get any of the examples to work.
Other than changing the GPIO's to match the board, what else do I need to change to use the MCAN peripheral examples with the launchpad?
Is there a set of MCAN examples that work with this launchpad?