Part Number: TMS320F280049C
Other Parts Discussed in Thread: C2000-CGT
Tool/software:
According to the C11 standard the following initialization should be valid:
#include <uchar.h>
#include <stdint.h>
const char16_t abc[] = u"This is supposed to work without throwing warnings..\n";
But when I try to compile it, I get the following warning:
$ ../C2000-CGT/bin/cl2000 --c11 -I../C2000-CGT/include test.c
"test.c", line 3: error: a value of type "unsigned short [54]" cannot be used to initialize an entity of type "const char16_t []"
1 error detected in the compilation of "test.c".
>> Compilation failure
The root cause is that if we follow the typedef chain back through least_uint16_t to __uint16_t, we find that for the CLA it is defined correctly, as unsigned short; but for the C2000, it is incorrectly defined as unsinged int. Even though these are the same thing, the compiler hates life and gives up.
I can make this code work by modifying it as follows:
#include <uchar.h>
#include <stdint.h>
const char16_t * abc = (char16_t *)u"This is supposed to work without throwing warnings..\n";
And while this compiles without errors, I can no longer use sizeof(abc) since it is now just a pointer. So it would appear there is no way to initialize a char16_t array.
If I do the unspeakable and force the definition of least_uint16_t to unsigned short (include/machine__types.h) jinstead of unsigned int, then lo and behold, the original example compiles without errors. I have no idea what else breaks when I do this, but just wanted to demonstrate that this is the root cause.
So the compiler apparently resolves u"This is UTF-16 text" to unsigned short, but char16_t resolves to unsigned int. Ironically, these are the same size, but one is a 16-bit integer intentionally, the other just happens to be that size; they are not the same.
The only time the type of char16_t matters is when defining UTF-16 strings, so I propose that either u"asdf" resolves to unsigned int, or least_uint16_t should resolve to unsigned short. Why on earth would it not?
Is there another syntax I could use for defining UTF-16 strings? A compiler option which magically makes this work? Is it safe to #define _CHAR16_T_DECLARED before including any system headers and to typedef unsigned short char16_t?
Any guidance would be appreciated.