Other Parts Discussed in Thread: CONTROLSUITE
I bought the 28069 USB controlStick kit last week. I installed the software (controlSUITE and CCSv5) and was up and running with the example projects in a matter of minutes. I had no problems and everything worked perfectly. After a bit of messing around with the projects (trying to incorporate CLA functionality into one of the example projects) the example project that I was working with was a mess, and I wanted to restore it to its original state. I tried to get them off the installation disk, but it didn't work. I reinstalled the controlSuite software, and that didn't work. I uninstalled and reinstalled, and that didn't work. I erased controlSuite and CCSv5 off the disk and reinstalled, and that finally got the project to restore to its original state, but now CCSv5 is complaining about all kinds of errors including RAM address ranges being incorrect, compiler versions not suported or not installed, include.h files not found, etc. Any further attempts to uninstall and reinstall do not help and I have very little hope of salvaging it. I would very much like to completely start over with this kit, since it worked flawlessly when I first installed it. Can anyone please help me wipe this installation off my disk so I can start fresh?
Thank you,
Justin