Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039: C2000 microcontrollers forum

Part Number: TMS320F280039

Tool/software:

Hi experts

please recommend C2000 devices with more than 100pin that meet the specifications below.

1. MCU spec

- one MCU controls two motors simultaneously or separately.

- core speed above 120Mhz

2. eQEP : 2ch

3. eCAP : 2ch

4. TripZone : Minimum 3ch

5. PWM : 8ch, PWM interrupt control period should be short. FSW is up to 16khz.

6. ADC : 12ch, ADCs up to 3channel should be capable of simultaneous sampling.  

7. CAN FD : 1ch , above 2Mbps

8. SPI : 1ch

9. SCI : 2ch

10. I2C : 1ch

11. GPIO : above 23ea

thanks