Part Number: TMS320F280039
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi experts
please recommend C2000 devices with more than 100pin that meet the specifications below.
1. MCU spec
- one MCU controls two motors simultaneously or separately.
- core speed above 120Mhz
2. eQEP : 2ch
3. eCAP : 2ch
4. TripZone : Minimum 3ch
5. PWM : 8ch, PWM interrupt control period should be short. FSW is up to 16khz.
6. ADC : 12ch, ADCs up to 3channel should be capable of simultaneous sampling.
7. CAN FD : 1ch , above 2Mbps
8. SPI : 1ch
9. SCI : 2ch
10. I2C : 1ch
11. GPIO : above 23ea
thanks