Part Number: TMS320F280033
Hi Champ,
I am asking for my customer. A follow-up on this post
In the post, it was answered to an detailed way to modify the registers for boot and the flash entry point.
To make it easier for user, we should able to modify flash entry point address for F280033 with DCSM as below setup then program the OTP, right ? To get the same result from above post. Also, the correct .cmd for F280033 is needed as well here.
Customer's HW GPIO24 & GPIO32 are designed pull up directly.

BTW, the checkbox for Zone 1 LINKPOINTER + Zone Select block is checked, while nothing is modified in there.
(1). That's all I need, right ? Anything else is needed ?
(2). Since GPIO24 & GPIO32 are pull-up in HW, I could leave the other three BOOTDEFx (x=0~2) there, right ?
Thanks for the support.
Regards,
Johnny