This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: MCU is getting RESET at 10ms

Part Number: TMS320F28379D
Other Parts Discussed in Thread: UNIFLASH

Hello Forms,

When +12V given to MCU identified that MCU rest pin Toggled such that I couldn't Flash any code into it.

Even tried using with UNIFLASH, but failed.


When Observed using Oscilloscope identified that for Every 10ms there is a drop for 56us drop.

Here is the Power Supply Schematic.
image.png

Here are images related to MCU Reset.

A) Turn Off Time : 56.4us

WhatsApp Image 2025-11-22 at 1.58.03 PM (1).jpeg

B) Turn ON Time : 10ms
WhatsApp Image 2025-11-22 at 1.58.03 PM.jpeg


Thanks in Advance,
Soumitri Kumar