Part Number: TMS320F28388D
Other Parts Discussed in Thread: UNIFLASH
Hello,
I am working on a custom PCB that uses the TMS320F28388D controller. I am able to flash the controller successfully using an XDS110 debugger through Code Composer Studio, which generates a .out file. I can also flash this .out file using UniFlash without any issues.
However, I need to flash the controller using a .hex file instead. When I generate a .hex file and try to flash it through UniFlash, the flashing process completes, but the code does not run on the controller. It seems the controller is not working with the .hex file.
.out file size: 1192 KB
.hex file size: 254 KB
I have created the .hex file using C2000 Hex Utility:
Thanks.