This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: CLB clock configuration

Part Number: TMS320F28388D

Hello, I have referred f28388D TRM, as per TRM CLB clock configuration shown below.

image.png

Here as shown there are two inputs 1) AUXPLL 2)SYSCLK
1) which register needs to be configure to define the clock input from above two sources.

2) while in TRM it is showing  2 possible inputs, in syscfg, it only showing AUXPLL as an input

image.png

3) By enabling SYNC (via CLKMODECLB1 ), it ensure phase alignment with SYSCLK or some additional features w.r.t. case where SYNC is disabled.

 

Regards