Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28P550SJ: MCAN troubleshooting issue

Part Number: TMS320F28P550SJ

 

I would like to start this new thread To ask for assistance. We have come across with some troubleshooting issues while bringing up our prototype. In specific, with the MCAN module. In the past, the MCAN module has been treated more like a blackbox module where we configured the speeds, and parameters we needed for our transmission and test whether messages are sent. However, this is a poor approach because whenever a single part of the configuration was not properly set up, we did see no messages being sent through CAN. 
  • Several points of failure produced the same output. We would like to have a deeper understanding with this peripheral. 
  • Another variable that could throw questions and problems was that we are using a PCAN so we can read to the other end, providing another failing point as the pcan may not be configured properly either to match our prototype can speed. 
Thus, we would like to know how you would recommend troubleshooting MCAN module without the need of another CAN device. If possible, we would like an in-depth guide on understanding better the peripheral registers so we could analyse them and extract which part of the configuration is not properly configured afterwards. 
 
To add more information, the process I am currently using is the following:
  • Calculate sampling point with timing bit calculator excel provided by ti
  • Put configuration in both a PCAN and MCU
  • From this point, I can only know if there are messages being received by PCAN, but the failure points are several. Therefore, I can only juggle with these questions by following a process of trial and error:
    • Is the bit timing config properly set? I can just check the excel of bit timing calculation and check that the MCAN registers of bit timing are confgirued.
    • Is the line delay affecting? Is properly configured the TDC register? Do not have any calculactions on which values should I select
    • Is the clock properly set up? A part from checking the registers, we do not know if exists another way to be certain that the expect MCAN clock config is porperly set.
  • If I am not receiving messages, the config is not ok. If after playing around with the aforementioned points, I hook up thew oscilloscope and try to measure the bit times, the messages do not make sense. The issue here is that when the config is not working I am only seeing error messages at a periodicty of 50us which indicated (ACK and Form errors) instead of our expected dummy message with a totally different periodicity. Therfore, we are out of ideas on how to analize the messages being sent thorugh CAN in order to detect the problems in the peripheral.
    • Ususally, when this happens is that the reciever node is not able to properly set the ACK bit in the message and the form error usually indicates that the bit timings are not properly configured.
My las finding, makes me think of the following question:
  • After debugging the issue during all day, I have detected that the bit timing in our prototype is not as good as expected. I have detected an arbitration time of about 800ns for a 1MHz speed and about 160ns for a 5MHz speed. I am wondering if the issue is the main clock that feed the system. Can it be possible that by using the internal oscillator, the can clock exceeds the oscillator tolerance and therefore, the other CAN nodes are not able to sample properly the messages?
 
Finally, It would be very appreciated any kind of literature that could help us to have a deeper understanding on the MCAN module and the CAN network.
 
Regards,
David