Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2800157: Facing Module over current Fault

Part Number: TMS320F2800157

Hi, please refer this data, module overcurrent fault is occuring in different test scenarios. could you please help us to analyse and to find root cause to resolve this issue.

Gain≈12.72 as per our circuit

Vmax =3.3v

Vsmax= Vmax/Gain=3.3/12.72 =0.2594339622641509

Imax=Vsmax/Rshunt=0.2594339622641509 / 0.0003

I(full scale current)= 864.77A

 

overCurrent_A =

   (objSets->overCurrent_A > objSets->maxPeakCurrent_A) ?

     objSets->maxPeakCurrent_A : objSets->overCurrent_A;

 

USER_MOTOR1_OVER_CURRENT_A = 500.0 A

USER_M1_ADC_FULL_SCALE_CURRENT_A = 864.888 A

objSets->maxPeakCurrent_A = 864.888 * 0.475 = 410.82 A

0.475 = safety margin factor

overCurrent_A = min(500 , 410.82)

overCurrent_A = 410.82 A

 

objSets->currentInv_sf = 4096 / USER_M1_ADC_FULL_SCALE_CURRENT_A;

currentInv_sf=4096/864.888=4.735

 

cmpValue = overCurrent_A * currentInv_sf;

cmpValue=410.82×4.735≈1944

 

410.82 A → 1944 ADC counts

 

You are in three-shunt mode:

USER_M1_IS_OFFSET_CMPSS = (2048+2048+2048)/3 = 2048

 

dacCMPValH = 2048 + 1944 = 3992

dacCMPValL = 2048 - 1944 = 104

 

CMPSS_setDACValueHigh(..., 3992);

CMPSS_setDACValueLow (..., 104);

 

CMPSS is set to trip when: ADC < 104   OR   ADC > 3992
Screenshot 2026-02-06 171437.png