This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F29H85X-SOM-EVM: Flashing and Debugging issue

Part Number: F29H85X-SOM-EVM
Other Parts Discussed in Thread: HSEC180ADAPEVM, TMDSHSECDOCK, , XDS110ISO-EVM

Hello,
We are using the F29H85X-SOM-EVM for developing our project with all the required additonal components such as TMDSHSECDOCK, HSEC180ADAPEVM and XDS110ISO-EVM.
I am using CPU1 and CPU3.

When I start the debugging my steps are such as below:
1- Start Project-less Debug
2-CPU1 "Connect Target"
3-Run-Load Program-Load CPU1.out 
4- Run CPU1 - it halts and waits for the CPU3 via ICP
5- CPU3 Connect target
6- Run-Load symbol- LoadCPU3.out
7- Run CPU3 and Run CPU1.

Now, although this sequence is working fine sometimes but, when I try to re-start this sequence there might errors pops up such as attached screenshot.

image.png

After this screnshot occurs, nothing happens the IDE just stuck there.

Then, i need to close the IDE, remove and reconnect the DOCK and XDS110ISO-EVM power conenctions. Even, sometimes I needed to restart the whole windows to succesfully debug again.

I am not sure what is the problem here is but this affects the studying a lot obviously because we can not focus on our SW related issues because we can not be connected the device!!!.

I have used CCS 12.6 a lot for F28 family device and nothing happened like this.

Please help us about this.