Part Number: TMS320F28054F-Q1
Other Parts Discussed in Thread: TMS320F28054F, UNIFLASH
Hi Experts,
I'm using a TMS320F28054F with InstaSpin.
- User application is placed in Zone 1 (Z1)
- InstaSpin project already includes Z1 DCSM-related sections in the linker command file (.cmd)
I attempted the following:
- Added a custom DCSM .asm file to program Z1 passwords
- Build completed successfully
- However, programming fails (via CCS / flash tool)
- If I remove the .asm file, download works normally
For comparison:
- On TMS320F280040C, using dcsm.cmd + dcsm.asm works correctly and DCSM is applied
My questions:
1. Does InstaSpin internally use or reserve Z1 DCSM (OTP)?
2. Is it possible to apply Z1 password protection on top of InstaSpin while keeping user code in Z1?
3. Or is it mandatory to move user application to Z2 when using DCSM with InstaSpin?
If needed, I can share error logs.
Thanks.