Part Number: F29H850TU
Hi,
I am using AI assisted development and came across the problem with muticore debug. It seems your MCP does not provide relevant functions.
This is hint I got from the AI agent:
-
Accordion summary...
What doesn't work:
-
connectTargettakes no parameter to specify which core to connect. In this multi-core session (CPU1, CPU2, CPU3, Cortex_M4_0 all visible vialistCores), calling it only ever reports "already connected" — referring to whichever core was implicitly connected by the original launch (CPU1). There's no way to direct it at a different core from the list. -
loadProgramandloadSymbolsdo accept an optionalcoreIdparameter. I passedcoreId: 2(CPU3's index) to both, and both failed:loadProgram→"Target must be connected before calling the function"/"Could not load file"loadSymbols→"Could not load file"
So the
coreIdparameter on these two tools doesn't actually succeed in targeting/connecting a different core — the session stays locked to whatever was connected at launch.
Jozef -