Hello,
I am using the TMDSHVMTRPFC development kit with CCSv5, and am running the example project "Sensored Field Oriented Control of 3-Phase Induction Motors, v1.1 February 2010". I believe this document was written for use with CCSv4.
To view variable in the Dual Time graph window, the document says to set the Start Address A and Start Address B to DLOG_4CH_buff1 and DLOG_4CH_buff2. This works for me when I use the C2000 compiler v5.2.2. However, when I switch to compiler v6.0, both start addresses don't work anymore. I searched through the project files, and cannot figure out what the start address is supposed to be.
I was using compiler v5.2.2 because it is compatible with Matlab/ Embedded Coder. For my current project, I am not using Embedded Coder, and there is always a warning that comes up saying that the project was originally built in a more recent compiler. Also, CCS kept locking up and not responding. I couldn't find any information about this problem from other forums. When I switched to v6.0, CCS seems to respond better, but now the data log address doesn't work.
Do you know if the Start address would change between compiler versions? If so, how do I find out what the address is?
Thank you,
Nick