This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Errors encountered during linking

Hello,

I am new to microcontrollers programming. I am using C2000 Microcontrollers Development tools with 320 F28069. I could build the example files available in the CCSv5 version. But when I attempted to build my project, I had few errors. They are:

Description	Resource	Path	Location	Type

#10010 errors encountered during linking; ArtificialLimbController_master C/C++ Problem
unresolved symbols remain		 	C/C++ Problem
unresolved symbol _RamfuncsLoadEnd, first referenced in ... C/C++ Problem
unresolved symbol _RamfuncsLoadStart, first referenced in ... C/C++ Problem
unresolved symbol _RamfuncsRunStart, first referenced in ... C/C++ Problem.
How can I fix these issues?.
Thank you.
  • Hi,

    Are you using FLASH? If yes you need to define these symbols in your linker command file as follows:

       ramfuncs                  : LOAD = FLASHAB,
                                   RUN = PRAMM1,
                                   LOAD_START(_RamfuncsLoadStart),
                                   LOAD_END(_RamfuncsLoadEnd),
                                   RUN_START(_RamfuncsRunStart),
                                   PAGE = 0

    where LOAD is the place where you programmed the .text section, and Run is the RAM Section where you want to load the code for runtime. MemCopy function will then copy the code from FLASH to RAM as defined with these symbols.

    Hope this helps

    Andreas

  • Hello,

    sorry, but I have not completely understood your answer. How can I get the RAM section that I use to load the code for runtime?

    It looks like this

    MEMORY
    {
    PAGE 0 :
    /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
    RAML0 : origin = 0x008000, length = 0x000800 /* on-chip RAM block L0 */
    RAML1 : origin = 0x008800, length = 0x000400 /* on-chip RAM block L1 */
    RAML3 : origin = 0x009000, length = 0x001000 /* on-chip RAM block L3 */
    OTP : origin = 0x3D7800, length = 0x000400 /* on-chip OTP */

    FLASHH : origin = 0x3D8000, length = 0x004000 /* on-chip FLASH */
    FLASHG : origin = 0x3DC000, length = 0x004000 /* on-chip FLASH */
    FLASHF : origin = 0x3E0000, length = 0x004000 /* on-chip FLASH */
    FLASHE : origin = 0x3E4000, length = 0x004000 /* on-chip FLASH */
    FLASHD : origin = 0x3E8000, length = 0x004000 /* on-chip FLASH */
    FLASHA : origin = 0x3F4000, length = 0x003F80 /* on-chip FLASH */
    CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
    BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
    CSM_PWL_P0 : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */

    FPUTABLES : origin = 0x3FD860, length = 0x0006A0 /* FPU Tables in Boot ROM */
    IQTABLES : origin = 0x3FDF00, length = 0x000B50 /* IQ Math Tables in Boot ROM */
    IQTABLES2 : origin = 0x3FEA50, length = 0x00008C /* IQ Math Tables in Boot ROM */
    IQTABLES3 : origin = 0x3FEADC, length = 0x0000AA /* IQ Math Tables in Boot ROM */

    ROM : origin = 0x3FF3B0, length = 0x000C10 /* Boot ROM */
    RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */
    VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */

    PAGE 1 : /* Data Memory */
    /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
    /* Registers remain on PAGE1 */

    BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */
    RAMM0 : origin = 0x000050, length = 0x0003B0 /* on-chip RAM block M0 */
    RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
    RAML2 : origin = 0x008C00, length = 0x000400 /* on-chip RAM block L2 */
    RAML4 : origin = 0x00A000, length = 0x008000 /* on-chip RAM block L4 merged together with L5, L6 and L7*/
    RAML8 : origin = 0x012000, length = 0x002000 /* on-chip RAM block L8 */
    FLASHB : origin = 0x3F0000, length = 0x004000 /* on-chip FLASH */
    FLASHC : origin = 0x3EC000, length = 0x004000 /* on-chip FLASH */
    CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080
    CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080
    }

    SECTIONS
    {
    /* Allocate program areas: */
    .cinit : > FLASHA PAGE = 0
    .pinit : > FLASHA, PAGE = 0
    .text : > FLASHA PAGE = 0
    codestart : > BEGIN PAGE = 0

    Cla1Prog : LOAD = FLASHD,
    RUN = RAML3,
    LOAD_START(_Cla1funcsLoadStart),
    LOAD_END(_Cla1funcsLoadEnd),
    RUN_START(_Cla1funcsRunStart),
    PAGE = 0

    Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 1
    CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 1

    ramfuncs : LOAD = FLASHD,
    RUN = RAML0,
    LOAD_START(_RamfuncsLoadStart),
    LOAD_END(_RamfuncsLoadEnd),
    RUN_START(_RamfuncsRunStart),
    PAGE = 0

     

  • Hi,

    I forgot - somewhere in your code you need to define

    extern Uint16 RamfuncsLoadStart;
    extern Uint16 RamfuncsLoadEnd;
    extern Uint16 RamfuncsRunStart;

    to tell the linker, that these symbols are defined somwhere outside your project.

    Prathamesh dhanpalwar said:
    sorry, but I have not completely understood your answer. How can I get the RAM section that I use to load the code for runtime?

    In your specific case, the code is loaded from FLASHD to RAML0

    Prathamesh dhanpalwar said:
    ramfuncs : LOAD = FLASHD,
    RUN = RAML0,
    LOAD_START(_RamfuncsLoadStart),
    LOAD_END(_RamfuncsLoadEnd),
    RUN_START(_RamfuncsRunStart),
    PAGE = 0

    BR Andreas

  • Hi Andreas,

    Ok. Thank you very much for your help.