This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XCLKOUT on eZdsp (F2812)

Hello All,

I am checking the XCLKOUT output on eZdsp.We have configured SYSCLK as 150MHZ.With the default configuration of XINT registers i am observing the XCLKOUT (p8 -- 29) frquency on scope(bandwidth 500MHZ).

Iam expecting as per TMS320x281x DSP External Interface datasheet the XCLKOUT frequency as SYSCLKOUT/4 = 150MHZ/4 = 37.5 MHZ. 

But iam observing that as 330HZ !!!(attached is screen shot of capture).Also the pulses looks like ramp signals.Is this ok?

Below are the values of XINTCNF2 contents watched in watch window

WRBUFF  00 
CLKMODE 1 
CLKOFF  0 
rsvd1   01 
WLEVEL  00 
MPNMC   0  
HOLD    0 
HOLDS   1 
HOLDAS  1  
rsvd2   0100  
XTIMCLK 001
rsvd3   0000000000000  

Is there any configuration that needs to be done to view XCLKOUT?

Kindly suggest.