This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SPI TMS320F240 in dSPACE

Hallo,

Im trying to read a 60 Bit Telegram using the SPI of a TMS320F240 Slave in a dSPACE 1104 plataform at 1.14 Mbitps.  Does anyone has experience with the access function developed by dSPACE for this? Im having a lot of problems to read the string. Recurrently I receive a "Alignment Error"  which could be because the functions are programmed to work with Bytes, as 60 Bits are 7,5 Bytes.I already ask in dSPACE support but they say they have difficulties to understand how a 60 Bit frame can be read, and also dont know why an Alignment Error occur.

Could be that the TMS320F240  consider the String lenght as 8 Bytes but the last nibble of the last Byte lost and therefore sends this "alignment Error". Does anyone have experience? I would be very glad for any help.

I send a picture of the 60 Bit Telegram i would like to read, with zoom on the first 12 Bits. Thanks for any help!