This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am seeing a floating point rounding condition (error??) that I do not expect. It causes a problem when two floats are added together and the resultant value is assigned to an integer. Here's the code snippet from my pwm configuration routine...
#define CLK_RATE_US 0.010 // 10 ns
float totalPrdTm_us; // pwm period
float t1Tm_us; // transistor 1 active time
float t2Tm_us; // transistor 2 active time
Uint16 totalPrdClks; // clocks in pwm period
t1Tm_us = .20;
t2Tm_us = .40;
totalPrdTm_us = t1Tm_us + t2Tm_us; // total period = 0.60 in watch window (float format)
// totalPrdTm_us as displayed in watch window in hex format is 0x3F199999
totalPrdClks = totalPrdTm_us / (float)CLK_RATE_US ; // result = 59, expect 60
totalPrdTm_us = 0.60; // total period
// totalPrdTm_us as displayed in watch window in hex format is 0x3F19999A
totalPrdClks = totalPrdTm_us / (float)CLK_RATE_US ; // result = 60, as expected
I can work around this by adding some very small value as follows:
totalPrdClks = totalPrdTm_us / (float)CLK_RATE_US + 0.0001;
This is annoying. I have checked this on another processor / compiler and the result of the addition results in the correct hex value of 0x3F19999A, and hence the correct final value of 60.
Is this the expected behavior of the CCS compiler?
This is a DSP/BIOS project running on the F28335 experimenter's kit.
CCS 3.3.82.13
Integrated Develpment 5.98.0.34
BIOS 5.33.04
Codgen 5.14
Silicon Rev 00.00.02
Regards,
Scott
In the hopes that this may help others, I got the following reply in response to providing the following additional info to tech support:
------------------------------------------------------------------------------------------
I did some more testing using the TI examples and also my own code. I
only get this problem when running in a DSP/BIOS project. To reproduce
most simply I used the Hello example at:
C:\CCStudio_v3.3\bios_5_33_04\packages\ti\bios\examples\basic\hello\ezdsp28335\hello.pjt
I added a few lines to the Hello.c file to reproduce the problem on an
F28335 Experimenter's Kit ...
Void main()
{
////////// START OF MY CODE/////////
#define CLOCK_RATE_US 0.010
Uint16 u1;
float f1, f2, f3;
f1 = 0.2;
f2 = 0.4;
f3 = f1 + f2;
u1 = (f1 + f2) / (float)CLOCK_RATE_US ; // u1 == 59
u1 = f3 / (float)CLOCK_RATE_US ; // u1 == 59
u1 = f3 / 0.01;
// u1 == 59
// This is my temporary work-around
f3 += 0.0001;
u1 = f3 / 0.01; // u1 == 60 CORRECT
/////////// END OF MY CODE///////
LOG_printf(&trace, "hello world!");
/* fall into DSP/BIOS idle loop */
return;
}
The actual c file is attached. I have also attached a pdf with relevant
info. If you need more info, let me know. I am at a loss at this point
but my guess would be that somehow I'm not linking in the correct fp
library (????).
Regards,
Scott
------------------------------------------------------------------------------------------------------------------------------
The tools team has accepted the defect (tracking # SDOCM00059580) and committed to fix for the next update of BIOS, v5.33.06. At this time I do not have a release date for this version, but when it is released it will be posted on the Update Advisor web site.
Texas Instruments
Software Technical Support