Other Parts Discussed in Thread: CONTROLSUITE
Hi,
I am using 28335 for SCI-A communication. I am able to get the first transmit interrupt, but later on i am not getting next interrupt for transmission of the next words in my buffer,.
Similarly, i am not getting any interrupt for reception. Please tell me what wrong am i doing.
My code -
/***************************************************************************************/
/* Imported header files: */
#include "DSP2833x_CpuTimers.h"
#include "scidrv.h"
#define BAUD_RATE_115200 115200
#define BAUD_RATE_9600 9600
#define MAX_SCIBUF_SIZE 256
#define LSPCLOCK 75000000
scidrv_txPacket_st scidrv_txPacket;
char *msgTxPtr_chp;
uint16_t msgFlag_u16 = 0;
static uint16_t wrIndx_u16s = 0;
static uint16_t rdIndx_u16s = 0;
static uint16_t readBuff_u16s[MAX_SCIBUF_SIZE];
static uint16_t writBuff_u16s[MAX_SCIBUF_SIZE];
/* Local Function Defines */
void scidrv_InitSci_vd(void);
static void scidrv_InitSciA_vd(void);
static void SetBaudRate_vds(uint16_t interface_u16,uint32_t sciBaudRt_u32);
static void scidrv_InitSciAGpio_vd(void);
static uint16_t HexToAscii(uint16_t hexValue_u16);
/*--------------------------------------------------------------------------------------*/
/*!@brief scidrv_InitSci_vd:Initializes the SCI A module for communication
---------------------------------------------------------------------------------------*/
void scidrv_InitSci_vd(void)
{
uint16_t index_u16 = 0;
/* Initialize the write buffer with data that has to be written to the SCI A*/
for(index_u16 = 0; index_u16 < MAX_SCIBUF_SIZE; index_u16++)
{
/* Initialize the write buffer with data that has to be written to the SCI A*/
writBuff_u16s[index_u16] = MAX_SCIBUF_SIZE - index_u16;
/* Initialize the read buffer with zero*/
readBuff_u16s[index_u16] = 0;
}
scidrv_InitSciA_vd();
EALLOW;
DINT;
PieVectTable.SCIRXINTA = &scidrv_ReceiveAIsr_vd;
PieVectTable.SCITXINTA = &scidrv_TransmitAIsr_vd;
EINT; // Enable CPU interrupt
EDIS;
}
/*-------------------------------------------------------------------------------------*/
/*!@brief scidrv_InitSciA_vd:This function initializes the SCI A module.
*-------------------------------------------------------------------------------------*/
void scidrv_InitSciA_vd(void)
{
EALLOW;
/* Initialize SCI-A for Debug interface */
/* Note: Clocks were turned on to the SCIA peripheral */
/* in the InitSysCtrl() function */
/* 1 stop bit, No loopback */
/* No parity,8 char bits,*/
/* async mode, idle-line protocol */
SciaRegs.SCICCR.all = 0x0007;
/* enable TX, RX, internal SCICLK,*/
/* Disable RX ERR, SLEEP, TXWAKE*/
SciaRegs.SCICTL1.all = 0x0003;
SciaRegs.SCICTL2.all = 0x0003;
SciaRegs.SCICTL2.bit.TXINTENA = 1; /*Enable TX interrupt*/
SciaRegs.SCICTL2.bit.RXBKINTENA = 1; /*Enable RX interrupt*/
SciaRegs.SCICTL1.all = 0x0023; /* Relinquish SCI from Reset*/
/* Added Function for Setting Baud rate for SCI-A*/
SetBaudRate_vds(SCIA, BAUD_RATE_115200);
/* Enable interrupts required for this example*/
PieCtrlRegs.PIEIER9.bit.INTx1=1; /* PIE Group 9, int1*/
PieCtrlRegs.PIEIER9.bit.INTx2=1; /* PIE Group 9, INT2*/
/* Enable interrupts required for SCI */
IER |= PIEACK_GROUP9;
EDIS;
scidrv_InitSciAGpio_vd();
}
/*-------------------------------------------------------------------------------------*/
/*!@brief SetBaudRate_svd:This function Sets Baud Rate for SCI Driver.
*-------------------------------------------------------------------------------------*/
static void SetBaudRate_vds(uint16_t interface_u16, uint32_t sciBaudRt_u32)
{
uint16_t brrDecVal_u16 = INIT_VAL;
brrDecVal_u16 = (LSPCLOCK/(sciBaudRt_u32 * EIGHT)) - ONE;
switch(interface_u16)
{
case SCIA:
SciaRegs.SCIHBAUD = (brrDecVal_u16 & 0xFF00) >> EIGHT_BIT;
SciaRegs.SCILBAUD = (brrDecVal_u16 & 0x00FF);
break;
case SCIB:
ScibRegs.SCIHBAUD = (brrDecVal_u16 & 0xFF00) >> EIGHT_BIT;
ScibRegs.SCILBAUD = (brrDecVal_u16 & 0x00FF);
break;
case SCIC:
ScicRegs.SCIHBAUD = (brrDecVal_u16 & 0xFF00) >> EIGHT_BIT;
ScicRegs.SCILBAUD = (brrDecVal_u16 & 0x00FF);
break;
default:
/* 2400 ~ 9600 bps */
/* 4801 ~ 9600 bps */
/* 9603 ~ 9600 bps */
/* 19230 ~ 9600 bps */
/* 38461 ~ 9600 bps */
/* 115384 ~ 115200 bps */
break;
}
return;
}
/*-------------------------------------------------------------------------------------*/
/*!@brief scidrv_InitSciAGpio_vd:This function initializes GPIO pins to
function as SCI-A pins
*-------------------------------------------------------------------------------------*/
void scidrv_InitSciAGpio_vd()
{
EALLOW;
/* Enable internal pull-up for the selected pins */
/* Pull-ups can be enabled or disabled disabled by the user. */
/* This will enable the pull-ups for the specified pins. */
GpioCtrlRegs.GPAPUD.bit.GPIO28 = SCI_PULLUP_EN; // Enable pull-up for GPIO28(SCIRXDA)
GpioCtrlRegs.GPAPUD.bit.GPIO29 = SCI_PULLUP_EN; // Enable pull-up for GPIO29(SCITXDA)
GpioCtrlRegs.GPADIR.bit.GPIO28 = 0;
GpioCtrlRegs.GPADIR.bit.GPIO29 = 1;
/* Set qualification for selected pins to asynch only */
/* Inputs are synchronized to SYSCLKOUT by default. */
/* This will select asynch (no qualification) for the selected pins. */
GpioCtrlRegs.GPAQSEL2.bit.GPIO28 = SCI_GPIO_ASYNC; // Asynch input GPIO28 (SCIRXDA)
GpioCtrlRegs.GPAQSEL2.bit.GPIO29 = SCI_GPIO_ASYNC; // Asynch input GPIO29 (SCITXDA)
/* Configure SCI-A pins using GPIO register */
/* This specifies which of the possible GPIO pins will be SCI functional pins. */
GpioCtrlRegs.GPAMUX2.bit.GPIO28 = SCIA_EN; // Configure GPIO28 for SCIRXDA operation
GpioCtrlRegs.GPAMUX2.bit.GPIO29 = SCIA_EN; // Configure GPIO29 for SCITXDA operation
EDIS;
}
/*--------------------------------------------------------------------------------------*/
/*!@brief test_SciADebugPort_vd:
---------------------------------------------------------------------------------------*/
void test_SciADebugPort_bool(void)
{
/* Write the data from write buffer to SCI*/
scidrv_transmit_vd(writBuff_u16s, MAX_SCIBUF_SIZE);
}
/*--------------------------------------------------------------------------------------*/
/*!@brief scidrv_TransmitAIsr_vd:Interrupt Service Routine for SCI-A transmission
---------------------------------------------------------------------------------------*/
void scidrv_TransmitAIsr_vd(void)
{
if(MAX_SCIBUF_SIZE > wrIndx_u16s)
{
// xmit MSB
SciaRegs.SCITXBUF = (HexToAscii(writBuff_u16s[++wrIndx_u16s] & 0xFF00) >> 8);
// xmit LSB
SciaRegs.SCITXBUF = (HexToAscii(writBuff_u16s[wrIndx_u16s] & 0x00FF));
EALLOW;
// SciaRegs.SCICTL2.bit.TXINTENA = 1;
SciaRegs.SCICCR.all = 0x0007;
SciaRegs.SCICTL1.all =0x0023; // Relinquish SCI from Reset
}
else
{
wrIndx_u16s = 0;
EALLOW;
SciaRegs.SCICTL2.bit.TXINTENA = 0;
SciaRegs.SCICTL1.bit.TXENA = 0;
}
PieCtrlRegs.PIEACK.all |= PIEACK_GROUP9; // Issue PIE ACK
EDIS;
}
/*--------------------------------------------------------------------------------------*/
/*!@brief scidrv_ReceiveAIsr_vd:Interrupt Service Routine for SCI-A transmission
---------------------------------------------------------------------------------------*/
void scidrv_ReceiveAIsr_vd(void)
{
uint16_t cmdByteRec_u16;
cmdByteRec_u16 = SciaRegs.SCIRXBUF.all;
readBuff_u16s[rdIndx_u16s] = cmdByteRec_u16;
if(rdIndx_u16s >= MAX_SCIBUF_SIZE)
rdIndx_u16s = 0;
if(((cmdByteRec_u16 != 255) && (cmdByteRec_u16 != 10)))
{
// MBX_post(&mbxdiag, &cmdByteRec_u16,0);
}
EALLOW;
/* Ack the Reception Interrupt*/
PieCtrlRegs.PIEACK.all |= PIEACK_GROUP9; // Issue PIE ack
EDIS;
}
/*--------------------------------------------------------------------------------------*/
/*!@brief This routine will extract the command from the command buffer and
* form a string.
---------------------------------------------------------------------------------------*/
void scidrv_transmit_vd(uint16_t *txDataptr_u16p, uint16_t length_u16)
{
uint16_t txData;
EALLOW;
// SciaRegs.SCICTL2.bit.TXINTENA = 1;
SciaRegs.SCICTL1.bit.TXENA = 1;
EDIS;
/* Set the message flag to 0 indicating the digit data is sent to terminal*/
msgFlag_u16 = 0;
/*Update the transmission data pointer and length */
scidrv_txPacket.dataPtr_u16p = txDataptr_u16p;
scidrv_txPacket.len_u16 = length_u16;
/* send one byte of data to initiate the data transmission*/
/* get the last nibble of the data*/
// txData = (((*txDataptr_u16p) & 0xF000) >> 12);
// txData = *txDataptr_u16p;
txData = (((*txDataptr_u16p) & 0xFF00) >> 8);
txData = 0x0061;
/* convert the digit to its ascii*/
// txData = HexToAscii(txData);
/* load the tx buffer*/
SciaRegs.SCITXBUF = txData;
GpioDataRegs.GPATOGGLE.bit.GPIO31 = 1;
return;
}
/*--------------------------------------------------------------------------------------*/
/*!@brief HextoAscii conversion:Convetrs a hex character to its equivalent ASCII
---------------------------------------------------------------------------------------*/
uint16_t HexToAscii(uint16_t hexValue_u16)
{
uint16_t asciiValue;
if(hexValue_u16 >= 0x0A)
{
asciiValue = hexValue_u16 - 0x0A;
asciiValue = asciiValue + 'A';
}
else
{
asciiValue = hexValue_u16 + '0';
}
return asciiValue;
}
//===========================================================================
// End of file.
//===========================================================================
Please help with appropiate suggestions.
Arpan