Other Parts Discussed in Thread: CONTROLSUITE
Hi,
When we use epwm8A-8B with gpio14-15 it works fine. But when we use it with gpio 60-61 itwe don't see anything from outputs but the counters are counting. Also we have the same problem with epwm9A-9B. epwm9 is working with gpio30-31 and not working with gpio62-63. What can cause this problem? We have tried the software with two different experimenters kits and with two of our custom design board. We see the same things. It can't be a coincidence taht all of the boards are broken, I suppose. Can you help us solve the problem?
Best Regards.