Hello,
I have loaded the dual core blinky example and upon reset the device only blinks the LED for the m3. This is the same behavior that is demonstrated when using my code. The C28 core does not execute the program when booted by the master system after reset.
For both projects the code works properly when the debugger is attached. I can verify that the IPC command to boot the dsp is completing without error when using my code.
Code Composer Studio
Version: 5.3.0.00090
IPC 1.25.01.09
xdctools 3.24.05.48
bios 6.34.04.22