This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC trigger on Concerto F28M36x



Hello there,

I am trying to build up on the 'adc_soc_c28' example on F28M36x, where i trigger the ADC conversion using the PWM module. Everything works fine if i trigger once per PWM period (zero or max). However, with the new ADC type i don't know how to configure the ADC in order to use both the PWM triggers SOCA and SOCB to achieve double the sampling per PWM period (zero and max).

Does anyone done it already for this DSP or other DSP with equivalent type (type 3 ADC)? Can you give some hints on how this task can be done?

PS: Using the the TMDXDOCK28M36 with TMS320F28M36 Concerto controlCARD R1.1.

Best regards,

Ionut

  • Hey Ionut,

    How many signals do you need to convert?  Can you do something like:

    ePWM1 SOCA triggered at first point in period

    ePWM1 SOCB triggered at second point in period

    ADCTRIG1 is ePWM1SOCA

    ADCTRIG2 is ePWM1SOCB

    SOC0-SOC7 are triggered from ADCTRIG1

    SOC0-SOC7 convert external signals 0-7

    SOC8-SOC15 are triggered from ADCTRIG2

    SOC8-SOC15 convert external signasl 0-7 (same channel mux selection as SOC0-SOC7).

    ------------

    Also, if you are using up-down count mode, it looks like SOCxSEL in the ePWM has the option of triggering on both zero and period (see table 7-84 in the TRM).

  • Hi Devin,

    Thank you for your fast reply. Something similar like you suggest i've tried, but i don't get the expected result. The ADC interrupt is running with the same frequency as the PWM interrupt, which should be double. Do i have to setup two interrupts for the same ADC module? I need to sample 3 signals only with double the PWM freq.

    I attach the ADC and PWM settings i make, maybe you can see something i am missing here.

    Best regards,

    Ionut

    _____ADC setup:

        EALLOW;
        // Enable non-overlap mode i.e. conversion and future sampling events don't overlap
        Adc1Regs.ADCCTL2.bit.ADCNONOVERLAP = 1;

        // ADCINT1 is generated after AdcResults latch
        Adc1Regs.ADCCTL1.bit.INTPULSEPOS   = 1;

        // Enabled ADCINT1
        Adc1Regs.INTSEL1N2.bit.INT1E       = 1;

        // Disable ADCINT1 Continuous mode
        Adc1Regs.INTSEL1N2.bit.INT1CONT    = 0;

        // Setup EOC0 to trigger ADCINT1
        Adc1Regs.INTSEL1N2.bit.INT1SEL     = 0;

        // Set SOC0 channel select to ADC1A0 - AC Current Phase U
        Adc1Regs.ADCSOC0CTL.bit.CHSEL      = 0;
        Adc1Regs.ADCSOC8CTL.bit.CHSEL      = 0;

        // Set SOC1 channel select to ADC1A2 - AC Current Phase V
        Adc1Regs.ADCSOC1CTL.bit.CHSEL      = 2;
        Adc1Regs.ADCSOC9CTL.bit.CHSEL      = 2;

        // Set SOC2 channel select to ADC1A4 - AC Current Phase W
        Adc1Regs.ADCSOC2CTL.bit.CHSEL      = 4;
        Adc1Regs.ADCSOC10CTL.bit.CHSEL      = 4;

        // Assigning EPWM1SOCA to ADC TRIGGER 1 of the ADC module
        AnalogSysctrlRegs.TRIG1SEL.all     = 5;
        AnalogSysctrlRegs.TRIG2SEL.all     = 6;

        // Set SOCs start trigger to ADC Trigger 1 (EPWM1 SOCA) of the ADC
        Adc1Regs.ADCSOC0CTL.bit.TRIGSEL    = 5;
        Adc1Regs.ADCSOC1CTL.bit.TRIGSEL    = 5;
        Adc1Regs.ADCSOC2CTL.bit.TRIGSEL    = 5;

        Adc1Regs.ADCSOC8CTL.bit.TRIGSEL    = 6;
        Adc1Regs.ADCSOC9CTL.bit.TRIGSEL    = 6;
        Adc1Regs.ADCSOC10CTL.bit.TRIGSEL    = 6;

        // Set SOC0-5 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1) - fastest
        Adc1Regs.ADCSOC0CTL.bit.ACQPS      = 6;
        Adc1Regs.ADCSOC1CTL.bit.ACQPS      = 6;
        Adc1Regs.ADCSOC2CTL.bit.ACQPS      = 6;
        Adc1Regs.ADCSOC8CTL.bit.ACQPS      = 6;
        Adc1Regs.ADCSOC9CTL.bit.ACQPS      = 6;
        Adc1Regs.ADCSOC10CTL.bit.ACQPS     = 6;

        EDIS;

    ___PWM setup:

        EALLOW;

        // Settings for ADC triggers (SOCA and SOCB)
        GpioG1CtrlRegs.GPADIR.bit.GPIO8        = 1;         // Set as output for SOCA
        GpioG1CtrlRegs.GPAMUX1.bit.GPIO8    = 3;         // Set MUX to ADCSOCAO

        GpioG1CtrlRegs.GPADIR.bit.GPIO10    = 1;         // Set as output for SOCB
        GpioG1CtrlRegs.GPAMUX1.bit.GPIO10    = 3;         // Set MUX to ADCSOCBO

        EDIS;

    ///////////////////////////// not relevant part deleted

        // Setup triggers for ADC interrupt in Zero (only by EPwm1)
        // Set SOCA for ADC during Zero event
        EPwm1Regs.ETSEL.bit.SOCAEN         = 1;      // Enable SOCA
        EPwm1Regs.ETSEL.bit.SOCASEL = ET_CTR_ZERO;   // Select SOCA on Zero event (TBCTR = 0x0000)
        EPwm1Regs.ETPS.bit.SOCAPRD         = 1;      // Generate interrupt on each period

        // Set SOCB for ADC during Max event
        EPwm1Regs.ETSEL.bit.SOCBEN            = 1;     // Enable SOCB
        EPwm1Regs.ETSEL.bit.SOCBSEL = ET_CTR_PRD;   // Select SOCB on MAX event (TBCTR = TBPRD)
        EPwm1Regs.ETPS.bit.SOCBPRD            = 1;     // Generate pulse on 1st event

  • Yeah, I think you need to duplicate the below code, but for ADCINT2 and triggered by SOC8.  You could point ADCINT2 to the same ISR is the PIE vector table, then look at which flag is set to determine where to grab the data from (or you could have 2 ISRs).

        // ADCINT1 is generated after AdcResults latch
        Adc1Regs.ADCCTL1.bit.INTPULSEPOS   = 1;

        // Enabled ADCINT1
        Adc1Regs.INTSEL1N2.bit.INT1E       = 1;

        // Disable ADCINT1 Continuous mode
        Adc1Regs.INTSEL1N2.bit.INT1CONT    = 0;

        // Setup EOC0 to trigger ADCINT1
        Adc1Regs.INTSEL1N2.bit.INT1SEL     = 0;

  • Hi Devin,

    Thank you very much for your help!

    I got the job done by using two interrupts as you suggested, running the same interrupt routine.

    Best regards,

    Ionut