Hi everyone,
I'm a student at an university of Grenoble - France and i actually make an internship on a F28M35x (F28M35H52C1) microcontroller ; i'm teaching use it with the workshop associated, and i'm arriving at the Lab 4-2 where we capteur an ePWM waveform with ADC.
...But to inspect ADC samples, we need to use a connector wire to connect 2 pins which is normally provided but i haven't got it !
So is it normal ? How can we compensate that ? i thought an iron cable or something like that to connect the pins considered, but i'm afraid to destroy the components with that.
Can you help me about that please ?