This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI,
I am now using the template “C:\ti\controlSUITE\development_kits\TemplateProjects\DPLibv3_4Template-F2803x” inside the controlSUITE on my F28069 Piccolo Experimenter Kit.
Initially, I set the duty cycle of the ePWM2 to be 0.2 at the main()
Duty2A =_IQ24(0.2);
And then I add one more line at C1 task:
void C1(void)
//------------------------------------------------------
{
Duty2A =_IQ24(0.6);
//-----------------
//the next time CpuTimer2 'counter' reaches Period value go to C2
C_Task_Ptr = &C2;
//-----------------
}
I observed from the CRO that the duty of ePWM2 is 0.6, which is expected.
And then, I would like to change the interrupt source of DPLib from ePWM2 Int to ePWM4 Int. I made the following changes:
The external variable and variable inside main.c
// PWMDRV_1ch
extern volatile long *PWMDRV_1ch_Duty4; // instance #2, EPWM4
volatile long Duty4A;
the init function of ePWM changed from 2 to 4
PWM_1ch_CNF(4, 300,0,0);
The init value inside main()
Duty4A =_IQ24(0.2);
The updated value inside C1 task:
Duty4A =_IQ24(0.6);
The Interrupt setting
// Set up C28x Interrupt
//Also Set the appropriate # define's in the {ProjectName}-Settings.h
//to enable interrupt management in the ISR
EALLOW;
PieVectTable.EPWM4_INT = &DPL_ISR; // Map Interrupt
EPwm4Regs.ETSEL.bit.SOCAEN = 1;
PieCtrlRegs.PIEIER3.bit.INTx4 = 1; // PIE level enable, Grp3 / Int4
EPwm4Regs.ETSEL.bit.INTSEL = ET_CTR_PRD; // INT on PRD event
EPwm4Regs.ETSEL.bit.INTEN = 1; // Enable INT
EPwm4Regs.ETPS.bit.INTPRD = ET_1ST; // Generate INT on every event
IER |= M_INT3; // Enable CPU INT3 connected to EPWM1-6 INTs:
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
EDIS;
The Init and the run time function inside ProjectName-DPL-ISR.asm
PWMDRV_1ch_INIT 4 ; PWM4A
…
PWMDRV_1ch 4 ; PWM4A
I observed from the CRO again and found that the duty of ePWM4 is 0.2 not 0.6, which implies the DPLib routine can only run one time, the updated value inside C1 task cannot be pass to the DPLib routine. I am pleasure if anyone can help, thank you.
Barry
Dear Gautam,
Attached please find the files.
BR,
Barry
//---------------------------------------------------------------------------------- // FILE: ProjectName-Main.c // // Description: Sample Template file to edit // The file drives duty on PWM1A using CLA and PWM2 using C28x // These can be deleted and modified by the user // CLA Task is triggered by the PWM 1 interrupt // C28x ISR is triggered by the PWM 2 interrupt // // Version: 3.4 // // Target: TMS320F2803x(PiccoloB) // //---------------------------------------------------------------------------------- // Copyright Texas Instruments �2004-2010 //---------------------------------------------------------------------------------- // Revision History: //---------------------------------------------------------------------------------- // Date | Description / Status //---------------------------------------------------------------------------------- // October 2012 - Sample template project with DPlibv3.4 (MB) //---------------------------------------------------------------------------------- // // PLEASE READ - Useful notes about this Project // Although this project is made up of several files, the most important ones are: // "{ProjectName}-Main.c" - this file // - Application Initialization, Peripheral configuration, // - Application management // - Slower background code loops and Task scheduling // "{ProjectName}-DevInit_F28xxx.c // - Device Initialization, e.g. Clock, PLL, WD, GPIO mapping // - Peripheral clock enables // - DevInit file will differ per each F28xxx device series, e.g. F280x, F2833x, // "{ProjectName}-CLA_Tasks.cla" // - Initialization code for DPlib CLA Macros // - CLA Task code // "{ProjectName}-Settings.h" // - Global defines (settings) project selections are found here // - This file is referenced by both C and ASM files. // "{ProjectName}-CLA_Shared.h" // - Variable defines and header includes that are shared between CLA and C28x // // Code is made up of sections, e.g. "FUNCTION PROTOTYPES", "VARIABLE DECLARATIONS" ,..etc // each section has FRAMEWORK and USER areas. // FRAMEWORK areas provide useful ready made "infrastructure" code which for the most part // does not need modification, e.g. Task scheduling, ISR call, GUI interface support,...etc // USER areas have functional example code which can be modified by USER to fit their appl. // // Code can be compiled with various build options (Incremental Builds IBx), these // options are selected in file "{ProjectName}-Settings.h". Note: "Rebuild All" compile // tool bar button must be used if this file is modified. //---------------------------------------------------------------------------------- //Uint64 #include "F2806x_Device.h" #include "ProjectName-CLA_Shared.h" #include "F2806x_EPwm_defines.h" #include "IQmathLib.h" //%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%% // FUNCTION PROTOTYPES //%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%% // Add prototypes of functions being used in the project here void DeviceInit(void); #ifdef FLASH void InitFlash(); #endif void MemCopy(); void CLA_Init(); //-------------------------------- DPLIB -------------------------------------------- void PWM_1ch_CNF(int16 n, Uint16 period, int16 mode, int16 phase); void ADC_SOC_CNF(int ChSel[], int Trigsel[], int ACQPS[], int IntChSel, int mode); // -------------------------------- FRAMEWORK -------------------------------------- // State Machine function prototypes //---------------------------------------------------------------------------------- // Alpha states void A0(void); //state A0 void B0(void); //state B0 void C0(void); //state C0 // A branch states void A1(void); //state A1 void A2(void); //state A2 void A3(void); //state A3 void A4(void); //state A4 // B branch states void B1(void); //state B1 void B2(void); //state B2 void B3(void); //state B3 void B4(void); //state B4 // C branch states void C1(void); //state C1 void C2(void); //state C2 void C3(void); //state C3 void C4(void); //state C4 // Variable declarations void (*Alpha_State_Ptr)(void); // Base States pointer void (*A_Task_Ptr)(void); // State pointer A branch void (*B_Task_Ptr)(void); // State pointer B branch void (*C_Task_Ptr)(void); // State pointer C branch //---------------------------------------------------------------------------------- //%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%% // VARIABLE DECLARATIONS - GENERAL //%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%% // -------------------------------- FRAMEWORK -------------------------------------- int16 VTimer0[4]; // Virtual Timers slaved off CPU Timer 0 int16 VTimer1[4]; // Virtual Timers slaved off CPU Timer 1 int16 VTimer2[4]; // Virtual Timers slaved off CPU Timer 2 // Used for running BackGround in flash, and ISR in RAM extern unsigned int RamfuncsLoadStart, RamfuncsLoadSize, RamfuncsRunStart; // Used for ADC Configuration int ChSel[16] = {0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0}; int TrigSel[16] = {0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0}; int ACQPS[16] = {8,8,8,8,8,8,8,8,8,8,8,8,8,8,8,8}; // Used to indirectly access all EPWM modules volatile struct EPWM_REGS *ePWM[] = { &EPwm1Regs, //intentional: (ePWM[0] not used) &EPwm1Regs, &EPwm2Regs, &EPwm3Regs, &EPwm4Regs, &EPwm5Regs, &EPwm6Regs, &EPwm7Regs, }; // Used to indirectly access all Comparator modules volatile struct COMP_REGS *Comp[] = { &Comp1Regs, //intentional: (Comp[0] not used) &Comp1Regs, &Comp2Regs, &Comp3Regs, }; // ---------------------------------- USER ----------------------------------------- // ---------------------------- DPLIB Net Pointers --------------------------------- // Declare net pointers that are used to connect the DP Lib Macros here // PWMDRV_1ch extern volatile long *PWMDRV_1ch_Duty4; // instance #2, EPWM2 // ---------------------------- DPLIB Variables --------------------------------- // Declare the net variables being used by the DP Lib Macro here // PWMDRV_1ch_CLA_C extern volatile float32 CLA_Duty1; // instance #1, EPWM1 volatile float Duty1A; volatile long Duty4A; //%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%% // VARIABLE DECLARATIONS - CCS WatchWindow / GUI support //%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%% // -------------------------------- FRAMEWORK -------------------------------------- //GUI support variables // sets a limit on the amount of external GUI controls - increase as necessary int16 *varSetTxtList[16]; //16 textbox controlled variables int16 *varSetBtnList[16]; //16 button controlled variables int16 *varSetSldrList[16]; //16 slider controlled variables int16 *varGetList[16]; //16 variables sendable to GUI int16 *arrayGetList[16]; //16 arrays sendable to GUI int16 LedBlinkCnt; // ---------------------------------- USER ----------------------------------------- // Monitor ("Get") // Display as: // Configure ("Set") // History arrays are used for Running Average calculation (boxcar filter) // Used for CCS display and GUI only, not part of control loop processing //Scaling Constants (values found via spreadsheet; exact value calibrated per board) // Variables for background support only (no need to access) int16 i; // common use incrementer Uint32 HistPtr, temp_Scratch; // Temp here means Temporary //%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%% // MAIN CODE - starts here //%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%% void main(void) { //================================================================================= // INITIALIZATION - General //================================================================================= // The DeviceInit() configures the clocks and pin mux registers // The function is declared in {ProjectName}-DevInit_F2803/2x.c, // Please ensure/edit that all the desired components pin muxes // are configured properly that clocks for the peripherals used // are enabled, for example the individual PWM clock must be enabled // along with the Time Base Clock DeviceInit(); // Device Life support & GPIO //-------------------------------- FRAMEWORK -------------------------------------- // Only used if running from FLASH // Note that the variable FLASH is defined by the compiler with -d FLASH #ifdef FLASH // Copy time critical code and Flash setup code to RAM // The RamfuncsLoadStart, RamfuncsLoadEnd, and RamfuncsRunStart // symbols are created by the linker. Refer to the linker files. memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (Uint32) &RamfuncsLoadSize); // MemCopy(&RamfuncsLoadStart, &RamfuncsLoadEnd, &RamfuncsRunStart); // Call Flash Initialization to setup flash wait-states // This function must reside in RAM InitFlash(); // Call the flash wrapper initialization function #endif //(FLASH) // Timing sync for background loops // Timer period definitions found in PeripheralHeaderIncludes.h CpuTimer0Regs.PRD.all = mSec1; // A tasks CpuTimer1Regs.PRD.all = mSec10; // B tasks CpuTimer2Regs.PRD.all = mSec100; // C tasks // Tasks State-machine init Alpha_State_Ptr = &A0; A_Task_Ptr = &A1; B_Task_Ptr = &B1; C_Task_Ptr = &C1; VTimer0[0] = 0; VTimer1[0] = 0; VTimer2[0] = 0; LedBlinkCnt = 5; // ---------------------------------- USER ----------------------------------------- // put common initialization/variable definitions here //=============================================================================== // INITIALIZATION - GUI connections //================================================================================= // Use this section only if you plan to "Instrument" your application using the // Microsoft C# freeware GUI Template provided by TI /* //"Set" variables //--------------------------------------- // assign GUI variable Textboxes to desired "setable" parameter addresses varSetTxtList[0] = &Gui_TxtListVar; varSetTxtList[1] = &Gui_TxtListVar; varSetTxtList[2] = &Gui_TxtListVar; varSetTxtList[3] = &Gui_TxtListVar; varSetTxtList[4] = &Gui_TxtListVar; varSetTxtList[5] = &Gui_TxtListVar; varSetTxtList[6] = &Gui_TxtListVar; varSetTxtList[7] = &Gui_TxtListVar; varSetTxtList[8] = &Gui_TxtListVar; varSetTxtList[9] = &Gui_TxtListVar; varSetTxtList[10] = &Gui_TxtListVar; varSetTxtList[11] = &Gui_TxtListVar; // assign GUI Buttons to desired flag addresses varSetBtnList[0] = &Gui_BtnListVar; varSetBtnList[1] = &Gui_BtnListVar; varSetBtnList[2] = &Gui_BtnListVar; varSetBtnList[3] = &Gui_BtnListVar; varSetBtnList[4] = &Gui_BtnListVar; // assign GUI Sliders to desired "setable" parameter addresses varSetSldrList[0] = &Gui_SldrListVar; varSetSldrList[1] = &Gui_SldrListVar; varSetSldrList[2] = &Gui_SldrListVar; varSetSldrList[3] = &Gui_SldrListVar; varSetSldrList[4] = &Gui_SldrListVar; //"Get" variables //--------------------------------------- // assign a GUI "getable" parameter address varGetList[0] = &Gui_GetListVar; varGetList[1] = &Gui_GetListVar; varGetList[2] = &Gui_GetListVar; varGetList[3] = &Gui_GetListVar; varGetList[4] = &Gui_GetListVar; varGetList[5] = &Gui_GetListVar; varGetList[6] = &Gui_GetListVar; varGetList[7] = &Gui_GetListVar; varGetList[8] = &Gui_GetListVar; varGetList[9] = &Gui_GetListVar; varGetList[10] = &Gui_GetListVar; varGetList[11] = &Gui_GetListVar; varGetList[12] = &Gui_GetListVar; varGetList[13] = &Gui_GetListVar; varGetList[14] = &Gui_GetListVar; varGetList[15] = &Gui_GetListVar; // assign a GUI "getable" parameter array address arrayGetList[0] = &DBUFF1; //only need to set initial position of array, arrayGetList[1] = &DBUFF2; // program will run through it accordingly arrayGetList[2] = &DBUFF3; arrayGetList[3] = &DBUFF4; */ //================================================================================== // INCREMENTAL BUILD OPTIONS - NOTE: selected via {ProjectName-Settings.h //================================================================================== // ---------------------------------- USER ----------------------------------------- //---------------------------------------------------------------------- #if (INCR_BUILD == 1) // Open Loop Two Phase Interleaved PFC PWM Driver //---------------------------------------------------------------------- // Configure PWM2 for 200Khz switching Frequency //Period Count= 60Mhz/200Khz = 300 PWM_1ch_CNF(4, 300,0,0); // Configure ADC to be triggered from EPWM1 Period event //Map channel to ADC Pin ChSel[0]=14; //Map channel 0 to pin ADC-B6 // for additional ADC conversions modify below /*ChSel[1]=n; //An ChSel[2]=n; //An ChSel[3]=n; //An ChSel[4]=n; //An ChSel[5]=n; //An ChSel[6]=n; //An ChSel[7]=n; //An ChSel[8]=n; //An ChSel[9]=n; //An ChSel[10]=n; //An ChSel[11]=n; //An ChSel[12]=n; //An ChSel[13]=n; //An ChSel[14]=n; //An ChSel[15]=n; //An */ // Select Trigger Event for ADC conversion TrigSel[0]= ADCTRIG_EPWM1_SOCA; // associate the appropriate peripheral trigger to the ADC channel /*TrigSel[1]= ADCTRIG_EPWMn_SOCA; TrigSel[2]= ADCTRIG_EPWMn_SOCA; TrigSel[3]= ADCTRIG_EPWMn_SOCA; TrigSel[4]= ADCTRIG_EPWMn_SOCA; TrigSel[5]= ADCTRIG_EPWMn_SOCA; TrigSel[6]= ADCTRIG_EPWMn_SOCA; TrigSel[7]= ADCTRIG_EPWMn_SOCA; TrigSel[8]= ADCTRIG_EPWMn_SOCA; TrigSel[9]= ADCTRIG_EPWMn_SOCA; TrigSel[10]= ADCTRIG_EPWMn_SOCA; TrigSel[11]= ADCTRIG_EPWMn_SOCA; TrigSel[12]= ADCTRIG_EPWMn_SOCA; TrigSel[13]= ADCTRIG_EPWMn_SOCA; TrigSel[14]= ADCTRIG_EPWMn_SOCA; TrigSel[15]= ADCTRIG_EPWMn_SOCA;*/ // Configure the ADC with auto interrupt clear mode // ADC interrupt after EOC of channel 0 ADC_SOC_CNF(ChSel,TrigSel,ACQPS,0,2); // Configure the EPWM1 to issue the SOC EPwm1Regs.ETSEL.bit.SOCAEN = 1; EPwm1Regs.ETSEL.bit.SOCASEL = ET_CTR_PRD; // Use PRD event as trigger for ADC SOC EPwm1Regs.ETPS.bit.SOCAPRD = ET_1ST; // Generate pulse on every event // Digital Power CLA(DP) library initialization DPL_CLAInit(); DPL_Init(); // Lib Module connection to "nets" //---------------------------------------- // Connect the PWM Driver input to an input variable, Open Loop System PWMDRV_1ch_Duty4 = &Duty4A; // Initialize the net variables CLA_Duty1 =(float32)(0.5); Duty4A =_IQ24(0.2); CLA_Init(); #endif // (INCR_BUILD == 1) //==================================================================================== // INTERRUPTS & ISR INITIALIZATION (best to run this section after other initialization) //==================================================================================== // Set Up CLA Task // Task 1 has the option to be started by either EPWM1_INT or ADCINT1 // In this case we will allow ADCINT1 to start CLA Task 1 EALLOW; // Configure PWM1 to issue interrupts EPwm1Regs.ETSEL.bit.INTSEL = ET_CTR_PRD; // INT on PRD event EPwm1Regs.ETSEL.bit.INTEN = 1; // Enable INT EPwm1Regs.ETPS.bit.INTPRD = ET_1ST; // Generate INT on every event Cla1Regs.MPISRCSEL1.bit.PERINT1SEL = CLA_INT1_EPWM1INT ; // 0=ADCINT1 1=none 2=EPWM1INT // Configure the interrupt that would occur each control cycles Cla1Regs.MIER.all = M_INT1; asm(" RPT #3 || NOP"); EDIS; // Set up C28x Interrupt //Also Set the appropriate # define's in the {ProjectName}-Settings.h //to enable interrupt management in the ISR EALLOW; PieVectTable.EPWM4_INT = &DPL_ISR; // Map Interrupt EPwm4Regs.ETSEL.bit.SOCAEN = 1; PieCtrlRegs.PIEIER3.bit.INTx4 = 1; // PIE level enable, Grp3 / Int2 EPwm4Regs.ETSEL.bit.INTSEL = ET_CTR_PRD; // INT on PRD event EPwm4Regs.ETSEL.bit.INTEN = 1; // Enable INT EPwm4Regs.ETPS.bit.INTPRD = ET_1ST; // Generate INT on every event IER |= M_INT3; // Enable CPU INT3 connected to EPWM1-6 INTs: EINT; // Enable Global interrupt INTM ERTM; // Enable Global realtime interrupt DBGM EDIS; //================================================================================= // BACKGROUND (BG) LOOP //================================================================================= //--------------------------------- FRAMEWORK ------------------------------------- for(;;) //infinite loop { // State machine entry & exit point //=========================================================== (*Alpha_State_Ptr)(); // jump to an Alpha state (A0,B0,...) //=========================================================== } } //END MAIN CODE /** * Configure hardware peripherals used by the CLA. */ void DPL_CLAInit(){ // Configure PWM1 for 200Khz switching Frequency // Period Count= 60Mhz/200Khz = 300 PWM_1ch_CNF(1, 300,1,0); } //================================================================================= // STATE-MACHINE SEQUENCING AND SYNCRONIZATION //================================================================================= //--------------------------------- FRAMEWORK ------------------------------------- void A0(void) { // loop rate synchronizer for A-tasks if(CpuTimer0Regs.TCR.bit.TIF == 1) { CpuTimer0Regs.TCR.bit.TIF = 1; // clear flag //----------------------------------------------------------- (*A_Task_Ptr)(); // jump to an A Task (A1,A2,A3,...) //----------------------------------------------------------- VTimer0[0]++; // virtual timer 0, instance 0 (spare) } Alpha_State_Ptr = &B0; // Comment out to allow only A tasks } void B0(void) { // loop rate synchronizer for B-tasks if(CpuTimer1Regs.TCR.bit.TIF == 1) { CpuTimer1Regs.TCR.bit.TIF = 1; // clear flag //----------------------------------------------------------- (*B_Task_Ptr)(); // jump to a B Task (B1,B2,B3,...) //----------------------------------------------------------- VTimer1[0]++; // virtual timer 1, instance 0 (spare) } Alpha_State_Ptr = &C0; // Allow C state tasks } void C0(void) { // loop rate synchronizer for C-tasks if(CpuTimer2Regs.TCR.bit.TIF == 1) { CpuTimer2Regs.TCR.bit.TIF = 1; // clear flag //----------------------------------------------------------- (*C_Task_Ptr)(); // jump to a C Task (C1,C2,C3,...) //----------------------------------------------------------- VTimer2[0]++; //virtual timer 2, instance 0 (spare) } Alpha_State_Ptr = &A0; // Back to State A0 } //================================================================================= // A - TASKS //================================================================================= //-------------------------------------------------------- void A1(void) //-------------------------------------------------------- { //------------------- //the next time CpuTimer0 'counter' reaches Period value go to A2 A_Task_Ptr = &A2; //------------------- } //----------------------------------------------------------------- void A2(void) //----------------------------------------------------------------- { //------------------- //the next time CpuTimer0 'counter' reaches Period value go to A1 A_Task_Ptr = &A3; //------------------- } //----------------------------------------- void A3(void) //----------------------------------------- { //----------------- //the next time CpuTimer0 'counter' reaches Period value go to A1 A_Task_Ptr = &A4; //----------------- } //---------------------------------------------------------- void A4(void) //--------------------------------------------------------- { //----------------- //the next time CpuTimer0 'counter' reaches Period value go to A1 A_Task_Ptr = &A1; //----------------- } //================================================================================= // B - TASKS //================================================================================= //----------------------------------- USER ---------------------------------------- //---------------------------------------- void B1(void) //---------------------------------------- { //----------------- //the next time CpuTimer1 'counter' reaches Period value go to B2 B_Task_Ptr = &B2; //----------------- } //---------------------------------------- void B2(void) // Blink LED on the control CArd //---------------------------------------- { if(LedBlinkCnt==0) { GpioDataRegs.GPBTOGGLE.bit.GPIO34 = 1; //turn on/off LD3 on the controlCARD LedBlinkCnt=5; } else LedBlinkCnt--; //----------------- //the next time CpuTimer1 'counter' reaches Period value go to B3 B_Task_Ptr = &B3; //----------------- } //---------------------------------------- void B3(void) //---------------------------------------- { //----------------- //the next time CpuTimer1 'counter' reaches Period value go to B4 B_Task_Ptr = &B4; //----------------- } //---------------------------------------- void B4(void) // SPARE //---------------------------------------- { //----------------- //the next time CpuTimer1 'counter' reaches Period value go to B1 B_Task_Ptr = &B1; //----------------- } //================================================================================= // C - TASKS //================================================================================= //--------------------------------- USER ------------------------------------------ //------------------------------------------------------ void C1(void) //------------------------------------------------------ { Duty4A =_IQ24(0.6); //----------------- //the next time CpuTimer2 'counter' reaches Period value go to C2 C_Task_Ptr = &C2; //----------------- } //---------------------------------------- void C2(void) //---------------------------------------- { //----------------- //the next time CpuTimer2 'counter' reaches Period value go to C3 C_Task_Ptr = &C3; //----------------- } //----------------------------------------- void C3(void) //----------------------------------------- { //----------------- //the next time CpuTimer2 'counter' reaches Period value go to C4 C_Task_Ptr = &C4; //----------------- } //----------------------------------------- void C4(void) // SPARE //----------------------------------------- { //----------------- //the next time CpuTimer2 'counter' reaches Period value go to C1 C_Task_Ptr = &C1; //----------------- }
Gautam Iyer said:Yes, the way you're updating the duty is erroneous. Can you attach the c file or screenshot?
Regards,
Gautam
Gautam Iyer said:Yes, the way you're updating the duty is erroneous. Can you attach the c file or screenshot?
Regards,
Gautam
//---------------------------------------------------------------------------------- // FILE: ProjectName-Main.c // // Description: Sample Template file to edit // The file drives duty on PWM1A using CLA and PWM2 using C28x // These can be deleted and modified by the user // CLA Task is triggered by the PWM 1 interrupt // C28x ISR is triggered by the PWM 2 interrupt // // Version: 3.4 // // Target: TMS320F2803x(PiccoloB) // //---------------------------------------------------------------------------------- // Copyright Texas Instruments �2004-2010 //---------------------------------------------------------------------------------- // Revision History: //---------------------------------------------------------------------------------- // Date | Description / Status //---------------------------------------------------------------------------------- // October 2012 - Sample template project with DPlibv3.4 (MB) //---------------------------------------------------------------------------------- // // PLEASE READ - Useful notes about this Project // Although this project is made up of several files, the most important ones are: // "{ProjectName}-Main.c" - this file // - Application Initialization, Peripheral configuration, // - Application management // - Slower background code loops and Task scheduling // "{ProjectName}-DevInit_F28xxx.c // - Device Initialization, e.g. Clock, PLL, WD, GPIO mapping // - Peripheral clock enables // - DevInit file will differ per each F28xxx device series, e.g. F280x, F2833x, // "{ProjectName}-CLA_Tasks.cla" // - Initialization code for DPlib CLA Macros // - CLA Task code // "{ProjectName}-Settings.h" // - Global defines (settings) project selections are found here // - This file is referenced by both C and ASM files. // "{ProjectName}-CLA_Shared.h" // - Variable defines and header includes that are shared between CLA and C28x // // Code is made up of sections, e.g. "FUNCTION PROTOTYPES", "VARIABLE DECLARATIONS" ,..etc // each section has FRAMEWORK and USER areas. // FRAMEWORK areas provide useful ready made "infrastructure" code which for the most part // does not need modification, e.g. Task scheduling, ISR call, GUI interface support,...etc // USER areas have functional example code which can be modified by USER to fit their appl. // // Code can be compiled with various build options (Incremental Builds IBx), these // options are selected in file "{ProjectName}-Settings.h". Note: "Rebuild All" compile // tool bar button must be used if this file is modified. //---------------------------------------------------------------------------------- //Uint64 #include "F2806x_Device.h" #include "ProjectName-CLA_Shared.h" #include "F2806x_EPwm_defines.h" #include "IQmathLib.h" //%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%% // FUNCTION PROTOTYPES //%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%% // Add prototypes of functions being used in the project here void DeviceInit(void); #ifdef FLASH void InitFlash(); #endif void MemCopy(); void CLA_Init(); //-------------------------------- DPLIB -------------------------------------------- void PWM_1ch_CNF(int16 n, Uint16 period, int16 mode, int16 phase); void ADC_SOC_CNF(int ChSel[], int Trigsel[], int ACQPS[], int IntChSel, int mode); // -------------------------------- FRAMEWORK -------------------------------------- // State Machine function prototypes //---------------------------------------------------------------------------------- // Alpha states void A0(void); //state A0 void B0(void); //state B0 void C0(void); //state C0 // A branch states void A1(void); //state A1 void A2(void); //state A2 void A3(void); //state A3 void A4(void); //state A4 // B branch states void B1(void); //state B1 void B2(void); //state B2 void B3(void); //state B3 void B4(void); //state B4 // C branch states void C1(void); //state C1 void C2(void); //state C2 void C3(void); //state C3 void C4(void); //state C4 // Variable declarations void (*Alpha_State_Ptr)(void); // Base States pointer void (*A_Task_Ptr)(void); // State pointer A branch void (*B_Task_Ptr)(void); // State pointer B branch void (*C_Task_Ptr)(void); // State pointer C branch //---------------------------------------------------------------------------------- //%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%% // VARIABLE DECLARATIONS - GENERAL //%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%% // -------------------------------- FRAMEWORK -------------------------------------- int16 VTimer0[4]; // Virtual Timers slaved off CPU Timer 0 int16 VTimer1[4]; // Virtual Timers slaved off CPU Timer 1 int16 VTimer2[4]; // Virtual Timers slaved off CPU Timer 2 // Used for running BackGround in flash, and ISR in RAM extern unsigned int RamfuncsLoadStart, RamfuncsLoadSize, RamfuncsRunStart; // Used for ADC Configuration int ChSel[16] = {0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0}; int TrigSel[16] = {0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0}; int ACQPS[16] = {8,8,8,8,8,8,8,8,8,8,8,8,8,8,8,8}; // Used to indirectly access all EPWM modules volatile struct EPWM_REGS *ePWM[] = { &EPwm1Regs, //intentional: (ePWM[0] not used) &EPwm1Regs, &EPwm2Regs, &EPwm3Regs, &EPwm4Regs, &EPwm5Regs, &EPwm6Regs, &EPwm7Regs, }; // Used to indirectly access all Comparator modules volatile struct COMP_REGS *Comp[] = { &Comp1Regs, //intentional: (Comp[0] not used) &Comp1Regs, &Comp2Regs, &Comp3Regs, }; // ---------------------------------- USER ----------------------------------------- // ---------------------------- DPLIB Net Pointers --------------------------------- // Declare net pointers that are used to connect the DP Lib Macros here // PWMDRV_1ch extern volatile long *PWMDRV_1ch_Duty4; // instance #2, EPWM2 // ---------------------------- DPLIB Variables --------------------------------- // Declare the net variables being used by the DP Lib Macro here // PWMDRV_1ch_CLA_C extern volatile float32 CLA_Duty1; // instance #1, EPWM1 volatile float Duty1A; volatile long Duty4A; //%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%% // VARIABLE DECLARATIONS - CCS WatchWindow / GUI support //%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%% // -------------------------------- FRAMEWORK -------------------------------------- //GUI support variables // sets a limit on the amount of external GUI controls - increase as necessary int16 *varSetTxtList[16]; //16 textbox controlled variables int16 *varSetBtnList[16]; //16 button controlled variables int16 *varSetSldrList[16]; //16 slider controlled variables int16 *varGetList[16]; //16 variables sendable to GUI int16 *arrayGetList[16]; //16 arrays sendable to GUI int16 LedBlinkCnt; // ---------------------------------- USER ----------------------------------------- // Monitor ("Get") // Display as: // Configure ("Set") // History arrays are used for Running Average calculation (boxcar filter) // Used for CCS display and GUI only, not part of control loop processing //Scaling Constants (values found via spreadsheet; exact value calibrated per board) // Variables for background support only (no need to access) int16 i; // common use incrementer Uint32 HistPtr, temp_Scratch; // Temp here means Temporary //%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%% // MAIN CODE - starts here //%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%% void main(void) { //================================================================================= // INITIALIZATION - General //================================================================================= // The DeviceInit() configures the clocks and pin mux registers // The function is declared in {ProjectName}-DevInit_F2803/2x.c, // Please ensure/edit that all the desired components pin muxes // are configured properly that clocks for the peripherals used // are enabled, for example the individual PWM clock must be enabled // along with the Time Base Clock DeviceInit(); // Device Life support & GPIO //-------------------------------- FRAMEWORK -------------------------------------- // Only used if running from FLASH // Note that the variable FLASH is defined by the compiler with -d FLASH #ifdef FLASH // Copy time critical code and Flash setup code to RAM // The RamfuncsLoadStart, RamfuncsLoadEnd, and RamfuncsRunStart // symbols are created by the linker. Refer to the linker files. memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (Uint32) &RamfuncsLoadSize); // MemCopy(&RamfuncsLoadStart, &RamfuncsLoadEnd, &RamfuncsRunStart); // Call Flash Initialization to setup flash wait-states // This function must reside in RAM InitFlash(); // Call the flash wrapper initialization function #endif //(FLASH) // Timing sync for background loops // Timer period definitions found in PeripheralHeaderIncludes.h CpuTimer0Regs.PRD.all = mSec1; // A tasks CpuTimer1Regs.PRD.all = mSec10; // B tasks CpuTimer2Regs.PRD.all = mSec100; // C tasks // Tasks State-machine init Alpha_State_Ptr = &A0; A_Task_Ptr = &A1; B_Task_Ptr = &B1; C_Task_Ptr = &C1; VTimer0[0] = 0; VTimer1[0] = 0; VTimer2[0] = 0; LedBlinkCnt = 5; // ---------------------------------- USER ----------------------------------------- // put common initialization/variable definitions here //=============================================================================== // INITIALIZATION - GUI connections //================================================================================= // Use this section only if you plan to "Instrument" your application using the // Microsoft C# freeware GUI Template provided by TI /* //"Set" variables //--------------------------------------- // assign GUI variable Textboxes to desired "setable" parameter addresses varSetTxtList[0] = &Gui_TxtListVar; varSetTxtList[1] = &Gui_TxtListVar; varSetTxtList[2] = &Gui_TxtListVar; varSetTxtList[3] = &Gui_TxtListVar; varSetTxtList[4] = &Gui_TxtListVar; varSetTxtList[5] = &Gui_TxtListVar; varSetTxtList[6] = &Gui_TxtListVar; varSetTxtList[7] = &Gui_TxtListVar; varSetTxtList[8] = &Gui_TxtListVar; varSetTxtList[9] = &Gui_TxtListVar; varSetTxtList[10] = &Gui_TxtListVar; varSetTxtList[11] = &Gui_TxtListVar; // assign GUI Buttons to desired flag addresses varSetBtnList[0] = &Gui_BtnListVar; varSetBtnList[1] = &Gui_BtnListVar; varSetBtnList[2] = &Gui_BtnListVar; varSetBtnList[3] = &Gui_BtnListVar; varSetBtnList[4] = &Gui_BtnListVar; // assign GUI Sliders to desired "setable" parameter addresses varSetSldrList[0] = &Gui_SldrListVar; varSetSldrList[1] = &Gui_SldrListVar; varSetSldrList[2] = &Gui_SldrListVar; varSetSldrList[3] = &Gui_SldrListVar; varSetSldrList[4] = &Gui_SldrListVar; //"Get" variables //--------------------------------------- // assign a GUI "getable" parameter address varGetList[0] = &Gui_GetListVar; varGetList[1] = &Gui_GetListVar; varGetList[2] = &Gui_GetListVar; varGetList[3] = &Gui_GetListVar; varGetList[4] = &Gui_GetListVar; varGetList[5] = &Gui_GetListVar; varGetList[6] = &Gui_GetListVar; varGetList[7] = &Gui_GetListVar; varGetList[8] = &Gui_GetListVar; varGetList[9] = &Gui_GetListVar; varGetList[10] = &Gui_GetListVar; varGetList[11] = &Gui_GetListVar; varGetList[12] = &Gui_GetListVar; varGetList[13] = &Gui_GetListVar; varGetList[14] = &Gui_GetListVar; varGetList[15] = &Gui_GetListVar; // assign a GUI "getable" parameter array address arrayGetList[0] = &DBUFF1; //only need to set initial position of array, arrayGetList[1] = &DBUFF2; // program will run through it accordingly arrayGetList[2] = &DBUFF3; arrayGetList[3] = &DBUFF4; */ //================================================================================== // INCREMENTAL BUILD OPTIONS - NOTE: selected via {ProjectName-Settings.h //================================================================================== // ---------------------------------- USER ----------------------------------------- //---------------------------------------------------------------------- #if (INCR_BUILD == 1) // Open Loop Two Phase Interleaved PFC PWM Driver //---------------------------------------------------------------------- // Configure PWM2 for 200Khz switching Frequency //Period Count= 60Mhz/200Khz = 300 PWM_1ch_CNF(4, 300,0,0); // Configure ADC to be triggered from EPWM1 Period event //Map channel to ADC Pin ChSel[0]=14; //Map channel 0 to pin ADC-B6 // for additional ADC conversions modify below /*ChSel[1]=n; //An ChSel[2]=n; //An ChSel[3]=n; //An ChSel[4]=n; //An ChSel[5]=n; //An ChSel[6]=n; //An ChSel[7]=n; //An ChSel[8]=n; //An ChSel[9]=n; //An ChSel[10]=n; //An ChSel[11]=n; //An ChSel[12]=n; //An ChSel[13]=n; //An ChSel[14]=n; //An ChSel[15]=n; //An */ // Select Trigger Event for ADC conversion TrigSel[0]= ADCTRIG_EPWM1_SOCA; // associate the appropriate peripheral trigger to the ADC channel /*TrigSel[1]= ADCTRIG_EPWMn_SOCA; TrigSel[2]= ADCTRIG_EPWMn_SOCA; TrigSel[3]= ADCTRIG_EPWMn_SOCA; TrigSel[4]= ADCTRIG_EPWMn_SOCA; TrigSel[5]= ADCTRIG_EPWMn_SOCA; TrigSel[6]= ADCTRIG_EPWMn_SOCA; TrigSel[7]= ADCTRIG_EPWMn_SOCA; TrigSel[8]= ADCTRIG_EPWMn_SOCA; TrigSel[9]= ADCTRIG_EPWMn_SOCA; TrigSel[10]= ADCTRIG_EPWMn_SOCA; TrigSel[11]= ADCTRIG_EPWMn_SOCA; TrigSel[12]= ADCTRIG_EPWMn_SOCA; TrigSel[13]= ADCTRIG_EPWMn_SOCA; TrigSel[14]= ADCTRIG_EPWMn_SOCA; TrigSel[15]= ADCTRIG_EPWMn_SOCA;*/ // Configure the ADC with auto interrupt clear mode // ADC interrupt after EOC of channel 0 ADC_SOC_CNF(ChSel,TrigSel,ACQPS,0,2); // Configure the EPWM1 to issue the SOC EPwm1Regs.ETSEL.bit.SOCAEN = 1; EPwm1Regs.ETSEL.bit.SOCASEL = ET_CTR_PRD; // Use PRD event as trigger for ADC SOC EPwm1Regs.ETPS.bit.SOCAPRD = ET_1ST; // Generate pulse on every event // Digital Power CLA(DP) library initialization DPL_CLAInit(); DPL_Init(); // Lib Module connection to "nets" //---------------------------------------- // Connect the PWM Driver input to an input variable, Open Loop System PWMDRV_1ch_Duty4 = &Duty4A; // Initialize the net variables CLA_Duty1 =(float32)(0.5); Duty4A =_IQ24(0.2); CLA_Init(); #endif // (INCR_BUILD == 1) //==================================================================================== // INTERRUPTS & ISR INITIALIZATION (best to run this section after other initialization) //==================================================================================== // Set Up CLA Task // Task 1 has the option to be started by either EPWM1_INT or ADCINT1 // In this case we will allow ADCINT1 to start CLA Task 1 EALLOW; // Configure PWM1 to issue interrupts EPwm1Regs.ETSEL.bit.INTSEL = ET_CTR_PRD; // INT on PRD event EPwm1Regs.ETSEL.bit.INTEN = 1; // Enable INT EPwm1Regs.ETPS.bit.INTPRD = ET_1ST; // Generate INT on every event Cla1Regs.MPISRCSEL1.bit.PERINT1SEL = CLA_INT1_EPWM1INT ; // 0=ADCINT1 1=none 2=EPWM1INT // Configure the interrupt that would occur each control cycles Cla1Regs.MIER.all = M_INT1; asm(" RPT #3 || NOP"); EDIS; // Set up C28x Interrupt //Also Set the appropriate # define's in the {ProjectName}-Settings.h //to enable interrupt management in the ISR EALLOW; PieVectTable.EPWM4_INT = &DPL_ISR; // Map Interrupt EPwm4Regs.ETSEL.bit.SOCAEN = 1; PieCtrlRegs.PIEIER3.bit.INTx4 = 1; // PIE level enable, Grp3 / Int2 EPwm4Regs.ETSEL.bit.INTSEL = ET_CTR_PRD; // INT on PRD event EPwm4Regs.ETSEL.bit.INTEN = 1; // Enable INT EPwm4Regs.ETPS.bit.INTPRD = ET_1ST; // Generate INT on every event IER |= M_INT3; // Enable CPU INT3 connected to EPWM1-6 INTs: EINT; // Enable Global interrupt INTM ERTM; // Enable Global realtime interrupt DBGM EDIS; //================================================================================= // BACKGROUND (BG) LOOP //================================================================================= //--------------------------------- FRAMEWORK ------------------------------------- for(;;) //infinite loop { // State machine entry & exit point //=========================================================== (*Alpha_State_Ptr)(); // jump to an Alpha state (A0,B0,...) //=========================================================== } } //END MAIN CODE /** * Configure hardware peripherals used by the CLA. */ void DPL_CLAInit(){ // Configure PWM1 for 200Khz switching Frequency // Period Count= 60Mhz/200Khz = 300 PWM_1ch_CNF(1, 300,1,0); } //================================================================================= // STATE-MACHINE SEQUENCING AND SYNCRONIZATION //================================================================================= //--------------------------------- FRAMEWORK ------------------------------------- void A0(void) { // loop rate synchronizer for A-tasks if(CpuTimer0Regs.TCR.bit.TIF == 1) { CpuTimer0Regs.TCR.bit.TIF = 1; // clear flag //----------------------------------------------------------- (*A_Task_Ptr)(); // jump to an A Task (A1,A2,A3,...) //----------------------------------------------------------- VTimer0[0]++; // virtual timer 0, instance 0 (spare) } Alpha_State_Ptr = &B0; // Comment out to allow only A tasks } void B0(void) { // loop rate synchronizer for B-tasks if(CpuTimer1Regs.TCR.bit.TIF == 1) { CpuTimer1Regs.TCR.bit.TIF = 1; // clear flag //----------------------------------------------------------- (*B_Task_Ptr)(); // jump to a B Task (B1,B2,B3,...) //----------------------------------------------------------- VTimer1[0]++; // virtual timer 1, instance 0 (spare) } Alpha_State_Ptr = &C0; // Allow C state tasks } void C0(void) { // loop rate synchronizer for C-tasks if(CpuTimer2Regs.TCR.bit.TIF == 1) { CpuTimer2Regs.TCR.bit.TIF = 1; // clear flag //----------------------------------------------------------- (*C_Task_Ptr)(); // jump to a C Task (C1,C2,C3,...) //----------------------------------------------------------- VTimer2[0]++; //virtual timer 2, instance 0 (spare) } Alpha_State_Ptr = &A0; // Back to State A0 } //================================================================================= // A - TASKS //================================================================================= //-------------------------------------------------------- void A1(void) //-------------------------------------------------------- { //------------------- //the next time CpuTimer0 'counter' reaches Period value go to A2 A_Task_Ptr = &A2; //------------------- } //----------------------------------------------------------------- void A2(void) //----------------------------------------------------------------- { //------------------- //the next time CpuTimer0 'counter' reaches Period value go to A1 A_Task_Ptr = &A3; //------------------- } //----------------------------------------- void A3(void) //----------------------------------------- { //----------------- //the next time CpuTimer0 'counter' reaches Period value go to A1 A_Task_Ptr = &A4; //----------------- } //---------------------------------------------------------- void A4(void) //--------------------------------------------------------- { //----------------- //the next time CpuTimer0 'counter' reaches Period value go to A1 A_Task_Ptr = &A1; //----------------- } //================================================================================= // B - TASKS //================================================================================= //----------------------------------- USER ---------------------------------------- //---------------------------------------- void B1(void) //---------------------------------------- { //----------------- //the next time CpuTimer1 'counter' reaches Period value go to B2 B_Task_Ptr = &B2; //----------------- } //---------------------------------------- void B2(void) // Blink LED on the control CArd //---------------------------------------- { if(LedBlinkCnt==0) { GpioDataRegs.GPBTOGGLE.bit.GPIO34 = 1; //turn on/off LD3 on the controlCARD LedBlinkCnt=5; } else LedBlinkCnt--; //----------------- //the next time CpuTimer1 'counter' reaches Period value go to B3 B_Task_Ptr = &B3; //----------------- } //---------------------------------------- void B3(void) //---------------------------------------- { //----------------- //the next time CpuTimer1 'counter' reaches Period value go to B4 B_Task_Ptr = &B4; //----------------- } //---------------------------------------- void B4(void) // SPARE //---------------------------------------- { //----------------- //the next time CpuTimer1 'counter' reaches Period value go to B1 B_Task_Ptr = &B1; //----------------- } //================================================================================= // C - TASKS //================================================================================= //--------------------------------- USER ------------------------------------------ //------------------------------------------------------ void C1(void) //------------------------------------------------------ { Duty4A =_IQ24(0.6); //----------------- //the next time CpuTimer2 'counter' reaches Period value go to C2 C_Task_Ptr = &C2; //----------------- } //---------------------------------------- void C2(void) //---------------------------------------- { //----------------- //the next time CpuTimer2 'counter' reaches Period value go to C3 C_Task_Ptr = &C3; //----------------- } //----------------------------------------- void C3(void) //----------------------------------------- { //----------------- //the next time CpuTimer2 'counter' reaches Period value go to C4 C_Task_Ptr = &C4; //----------------- } //----------------------------------------- void C4(void) // SPARE //----------------------------------------- { //----------------- //the next time CpuTimer2 'counter' reaches Period value go to C1 C_Task_Ptr = &C1; //----------------- }
Hello Barry!
I have looked at your C-file. It seems you do something wrong.
1
// Connect the PWM Driver input to an input variable, Open Loop System
PWMDRV_1ch_Duty4 = &Duty4A;
// Initialize the net variables
CLA_Duty1 =(float32)(0.5);// Why not 0.4?
Duty4A =_IQ24(0.2);// if you want 0.6 then you should paste Duty4A =_IQ24(0.6);
2
//Also Set the appropriate # define's in the {ProjectName}-Settings.h
//to enable interrupt management in the ISR
EALLOW;
PieVectTable.EPWM4_INT = &DPL_ISR; // Map Interrupt
EPwm4Regs.ETSEL.bit.SOCAEN = 1;// Why do you do that? This was not in the source file ProjectName-Main.c.
PieCtrlRegs.PIEIER3.bit.INTx4 = 1; // PIE level enable, Grp3 / Int2
EPwm4Regs.ETSEL.bit.INTSEL = ET_CTR_PRD; // INT on PRD event
EPwm4Regs.ETSEL.bit.INTEN = 1; // Enable INT
EPwm4Regs.ETPS.bit.INTPRD = ET_1ST; // Generate INT on every event
3
void C1(void)
//------------------------------------------------------
{
Duty4A =_IQ24(0.6);// You should comment this line
//-----------------
//the next time CpuTimer2 'counter' reaches Period value go to C2
C_Task_Ptr = &C2;
//-----------------
}
4
Maybe I don't understand what do you wish and I'm wrong.
Regards,
Igor
HI Igor,
Sorry that maybe I explain not clear. Let me describe the objective of the program:
The purpose of this program is to test whether the DPLib routine can execute or not during runtime. To verify this, I add Duty4A =_IQ24(0.2); inside the main() and Duty4A =_IQ24(0.6) inside the C1(). If the DPLib routine can execute, the duty cycle of that ePWM will eventually change to from 0.2 to 0.6.
At the beginning, I used ePWM1 and its interrupt to trigger the DPLib ISR. The duty is eventually changed to 0.6 observed by CRO.
And then, I would like to use ePWM4 and its interrupt to trigger the DPLib ISR. I changed all necessary variables and registers. This time, I found that the duty is 0.2 not 0.6.
Regarding Q2: EPwm4Regs.ETSEL.bit.SOCAEN = 1;// Why do you do that? This was not in the source file ProjectName-Main.c.
I tried comment and uncomment this code, the result is the same. The problem should not come from this line, please ignore.
Regarding Q2: CLA_Duty1 =(float32)(0.5);// Why not 0.4?, This is the duty of ePWM1 using CLA, the value of this will not affect this test.
BR,
Barry