Dear friends,
I have facing the target connection problem for c2000 piccolo launchpad (F28027 ) .wheather i am trying to connect ,it says
below error
can you please help me on this error.
regards
raju
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear friends,
I have facing the target connection problem for c2000 piccolo launchpad (F28027 ) .wheather i am trying to connect ,it says
below error
can you please help me on this error.
regards
raju
Hello Raju!
1 You can try to reinstall XDS100 drivers.
2 I would recommend you this thread http://e2e.ti.com/support/microcontrollers/c2000/f/171/p/268414/937959.aspx#937959
Regards,
Igor
XDS100v2 usb emulation i have get free with the board.
actually i have installed the Version: 5.4.0.00091 of code composer studio.still i am facing the same error..
what i have to i am not able to connect to my board.i have purchased two weeks back.
feel bad.not able to connect to board.
Dear friends,
when i connected manually,i have checked with piccolo f28027 emulation hardware.when i am going to test the connection
it says .dll file missing i have shown in attached snap shot.
and the error in notepad is.
[Start]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\DOCUME~1\ADMINI~1\LOCALS~1\APPLIC~1\.TI\
693494126\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioserdesusb.dll'.
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-600' (0xfffffda8).
The title is 'SC_ERR_LIB_ANY_LOCATE'.
The explanation is:
A required dynamic library could not be located.
The library isn't on the search path.
[End]
can you please tell me .how can i proceed to further.
Regards
Raju
Hi Raju!
I'm sorry. At your case I can suggest the reinstallation of all components (CCS + XDS100 driver) only and also I would recommend you to follow to my link mentioned above.
Regards,
Igor
Raju Bhai,
As Igor has mentioned, this is surely a driver conflict issue. Try uninstalling the complete CCS and its drivers. A proper fresh installation will solve your problem.
Regards,
Gautam
Thank you all,
yeah it's working for windows 7..but mine os is XP...for this i have did many times uninstallation...and installation.
No use..help it's asking the same as above.?
Regards
Raju
Hi Raju!
You can try to go through this link http://processors.wiki.ti.com/index.php/XDS100 (mainly Troubleshooting).
Regards,
Igor
Hi Raju,
This can also be a virus issue or malware issue. Check this link out:
http://pcsupport.about.com/od/findbyerrormessage/a/ftd2xx-dll-not-found-missing-error.htm
Regards,
Gautam
Hi Raju!
And just in case pay attention on these threads:
http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/287635.aspx
http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/286276.aspx
Regards,
Igor