This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ePWM



Hello.

I use F28M35H52C1 Concerto Control Card with dockStantion. Code Composer Studio Version: 5.5.0.00077.

Four days I tried launch PWM.  And I got some result, but not finished. Help me please =(. I don't understand where I made mistake.

My scope show me next signal from PWM1A :

But I set PERIOD =1000 and DUTY_CYCLE=500.

Below I attached my code:

/*
 * main.c
 */
#include "DSP28x_Project.h"     // Device Headerfile and Examples Include File

#define  DUTY_CYCLE     500
#define  PERIOD         1000

void ConfigEpwm1( void );

int main(void)
{

	// Step 1. Initialize System Control:
	// Enable Peripheral Clocks
	// This example function is found in the F28M35x_SysCtrl.c file.
	InitSysCtrl();
	// Step 2. Initalize GPIO:
	InitEPwm1Gpio();

	// Step 3. Clear all interrupts and initialize PIE vector table:
	// Disable CPU interrupts
	    DINT;

	// Disable CPU interrupts and clear all CPU interrupt flags:
	    IER = 0x0000;
	    IFR = 0x0000;

	    EALLOW;
	    SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0;       // Stop all the TB clocks
	    EDIS;

	    	ConfigEpwm1();

	    EALLOW;
	    SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1;        // Start all the timers synced
	    EDIS;

	    for(;;)
	    {
	        asm ("          NOP");
	    }

}

void ConfigEpwm1( void )
{
    // Assumes ePWM1 clock is already enabled in InitSysCtrl();
    EALLOW;
    // Configure PWM timers
    EPwm1Regs.TBPRD = PERIOD; // Period = 1201 TBCLK counts
    EPwm1Regs.TBPHS.half.TBPHS = 0; // Set Phase register to zero
    EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP; // Asymmetrical mode
    EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Phase loading disabled
    EPwm1Regs.TBCTL.bit.PRDLD = TB_SHADOW;
    EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_DISABLE;
    EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
    EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
    EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // load on CTR=Zero
    EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; // load on CTR=Zero
    EPwm1Regs.AQCTLA.bit.PRD = AQ_CLEAR;
    EPwm1Regs.AQCTLA.bit.CAU = AQ_SET;


    //EPwm1Regs.CMPC = DUTY_CYCLE;
    EPwm1Regs.CMPA.half.CMPA=DUTY_CYCLE;

//    EPwm1Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO;    // Select INT on Zero event
  //  EPwm1Regs.ETSEL.bit.INTEN = PWM1_INT_ENABLE; // Enable INT
    //EPwm1Regs.ETPS.bit.INTPRD = ET_1ST;          // Generate INT on 1st event

    EDIS;
}

And next code from M3:

int main(void)
{
    int i = 0;

    // Allow writes to protected registers.
    HWREG(SYSCTL_MWRALLOW) = 0xA5A5A5A5;

    // Sets up PLL, M3 running at 75MHz and C28 running at 150MHz
    SysCtlClockConfigSet(SYSCTL_USE_PLL | (SYSCTL_SPLLIMULT_M & 0xF) |
                         SYSCTL_SYSDIV_1 | SYSCTL_M3SSDIV_2 |
                         SYSCTL_XCLKDIV_4);

    // Enable all GPIOs
  //  PinoutSet();
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);

    // Enable Pullups on EPWM(1-8)A/B capable pins
    GPIOPadConfigSet(GPIO_PORTA_BASE, 0xFF, GPIO_PIN_TYPE_STD_WPU);
//    GPIOPadConfigSet(GPIO_PORTB_BASE, 0xFF, GPIO_PIN_TYPE_STD_WPU);

    // Give C28 control of all GPIOs
    GPIOPinConfigureCoreSelect(GPIO_PORTA_BASE, 0xFF, GPIO_PIN_C_CORE_SELECT);
    // Unlock the register to change the commit register value for Port B Pin 7
    // This disables the NMI functionality on the pin and allows other muxing 
    // options to be used
    HWREG(GPIO_PORTB_BASE+GPIO_O_LOCK) = GPIO_LOCK_KEY_DD;
    // Write to commit register
    HWREG(GPIO_PORTB_BASE+GPIO_O_CR) |= 0x000000FF;
    // Delay
    for (i=0;i<20;i++){};
    IPCMtoCBootControlSystem(CBROM_MTOC_BOOTMODE_BOOT_FROM_FLASH);

    // Disable clock supply for the watchdog modules
    SysCtlPeripheralDisable(SYSCTL_PERIPH_WDOG1);
    SysCtlPeripheralDisable(SYSCTL_PERIPH_WDOG0);
    //Enable processor interrupts.
    IntMasterEnable();

    // Main Code
    while(1) ;

}

  • Hi,

    Try using this example code:

    0601.epwm_adc_soc.zip

    Regards,

    Gautam

  • Dear Gautam .

    Thank you for your reply. I took this example and commented ADC and interrupt code. First, I would like get simplest PWM pulse,without ADC, interrupts etc. And got same result =( Below I attached my new code:

    #include "DSP28x_Project.h"       // Device Headerfile and Examples Include File
    #include <string.h>
    
    #define  DUTY_CYCLE     50000
    #define  PERIOD         100000
    
    // Prototype statements for functions found within this file.
    void ConfigEpwm1( void );
    
    main()
    {
    // Step 1. Initialize System Control for Control and Analog Subsytems
    // Enable Peripheral Clocks
    // This example function is found in the F28M35x_SysCtrl.c file.
        InitSysCtrl();
    
    // If project is linked into flash, copy critical code sections to RAM.
    #ifdef _FLASH
       memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);
    #endif
    
        EDIS;
    
    // Step 2. Initialize GPIO:
    // This example function is found in the F28M35x_Gpio.c file and
    // illustrates how to set the GPIO to it's default state.
    // InitGpio();  // Skipped for this example
        EALLOW;
        GpioG1CtrlRegs.GPADIR.bit.GPIO0  = 1;  // Set as output
          GpioG1CtrlRegs.GPAMUX1.bit.GPIO0 = 1;  // Select EPWM1SOCA as driving source
    
        EDIS;
    
    // Step 3. Clear all interrupts and initialize PIE vector table:
    // Disable CPU interrupts
        DINT;
    
    // Initialize the PIE control registers to their default state.
    // The default state is all PIE interrupts disabled and flags
    // are cleared.
    // This function is found in the F28M35x_PieCtrl.c file.
        InitPieCtrl();
    
    // Disable CPU interrupts and clear all CPU interrupt flags:
        IER = 0x0000;
        IFR = 0x0000;
    
    // Initialize the PIE vector table with pointers to the shell Interrupt
    // Service Routines (ISR).
    // This will populate the entire table, even if the interrupt
    // is not used in this example.  This is useful for debug purposes.
    // The shell ISR routines are found in F28M35x_DefaultIsr.c.
    // This function is found in F28M35x_PieVect.c.
    //    InitPieVectTable();
    
    // Interrupts that are used in this example are re-mapped to
    // ISR functions found within this file.
        EALLOW; // This is needed to write to EALLOW protected register
    //    PieVectTable.ADCINT1 = &adc1_isr;
        EDIS;   // This is needed to disable write to EALLOW protected registers
    
    // Step 4. Initialize all the Device Peripherals:
    // This function is found in F28M35x_InitPeripherals.c
    // InitPeripherals(); // Not required for this example
        //InitAdc1(); // For this example, init the ADC
    
    // Step 5. User specific code, enable interrupts:
    // Enable ADCINT1 in PIE
    //    PieCtrlRegs.PIEIER1.bit.INTx1 = 1;  // Enable INT 1.1 in the PIE
        IER |= M_INT1;                      // Enable CPU Interrupt 1
        EINT;                               // Enable Global interrupt INTM
        ERTM;                               // Enable Global realtime interrupt DBGM
    
    // Configure ADC and EPWM1 sub-modules
        ConfigEpwm1();
    
    // Wait for ADC interrupt
        for(;;)
        {
    
        }
    
    }
    void ConfigEpwm1( void )
    {
        // Assumes ePWM1 clock is already enabled in InitSysCtrl();
        EALLOW;
        // Enable SOCA and SOCB
    /*    EPwm1Regs.ETSEL.bit.SOCAEN         = 1;      // Enable SOC on A group
        EPwm1Regs.ETSEL.bit.SOCBEN         = 1;      // Enable SOC on B group
        EPwm1Regs.ETSEL.bit.SOCASEL        = 0x4;    // Select SOC from CMPA/CMPC on up count
        EPwm1Regs.ETSEL.bit.SOCBSEL        = 0x6;    // Select SOC from CMPB/CMPD on up count
        EPwm1Regs.ETSEL.bit.SOCASELCMP     = 0x1;    // CMPC
        EPwm1Regs.ETSEL.bit.SOCBSELCMP     = 0x1;    // CMPD
    
       EPwm1Regs.ETPS.bit.SOCAPRD         = 3;      // Generate SOCA pulse on every 3rd event
        EPwm1Regs.ETPS.bit.SOCBPRD         = 3;      // Generate SOCA pulse on every 3rd event
    /**/
        // Time-base registers
        EPwm1Regs.TBPRD = PERIOD;                    // Set EPWM timer period
        EPwm1Regs.TBPHS.all = 0;                     // Time-Base Phase Register
        EPwm1Regs.TBCTR = 0;                         // Time-Base Counter Register
        EPwm1Regs.TBCTL.bit.PRDLD = TB_IMMEDIATE;    // Set Immediate load
        EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP;   // Count-up mode: used for asymmetric PWM
    
        EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE;      // Disable phase loading
        EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_DISABLE;
    
        // Set TBCLK frequency
        EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;     // TBCLK = SYSCLKOUT
        EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1;
    
        // Setup shadow register load on ZERO
        EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
        EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
        EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // load on CTR=Zero
        EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; // load on CTR=Zero
    
        // Set Compare values
        EPwm1Regs.CMPC = DUTY_CYCLE;
        EPwm1Regs.CMPD = DUTY_CYCLE;
        EDIS;
    }

  • I got correct signal with one example.... tomorrow I'll trying to understand why it wasn't working =)  ... I'm thinking it was troubles with debugging mode, but not sure.

  • Hi Arthur,

    The code attached above was for ADC SOC than for generating ePWM. Her's the code for ePWM generation:

    //###########################################################################
    // FILE:   epwm_updown_aq_c28.c
    // TITLE:  Action Qualifier Module - Using up/down count.
    //
    //! \addtogroup control_example_list
    //! <h1> EPWM Action Qualifier (epwm_updown_aq)</h1>
    //!
    //! This example configures ePWM1, ePWM2, ePWM3 to produce an
    //! waveform with independant modulation on EPWMxA and
    //! EPWMxB.
    //!
    //! The compare values CMPA and CMPB are modified within the ePWM's ISR.
    //!
    //! The TB counter is in up/down count mode for this example.
    //!
    //! View the EPWM1A/B(PA0_GPIO0 & PA1_GPIO1), EPWM2A/B(PA2_GPIO2 & PA3_GPIO3)
    //! and EPWM3A/B(PA4_GPIO4 & PA5_GPIO5) waveforms via an oscilloscope.
    //
    //###########################################################################
    // $TI Release: F28M35x Support Library v201 $
    // $Release Date: Fri Jun  7 10:51:13 CDT 2013 $
    //###########################################################################
    
    #include "DSP28x_Project.h"     // Device Headerfile and Examples Include File
    
    typedef struct
    {
        volatile struct EPWM_REGS *EPwmRegHandle;
        Uint16 EPwm_CMPA_Direction;
        Uint16 EPwm_CMPB_Direction;
        Uint16 EPwmTimerIntCount;
        Uint16 EPwmMaxCMPA;
        Uint16 EPwmMinCMPA;
        Uint16 EPwmMaxCMPB;
        Uint16 EPwmMinCMPB;
    }EPWM_INFO;
    
    // Prototype statements for functions found within this file.
    void InitEPwm1Example(void);
    void InitEPwm2Example(void);
    void InitEPwm3Example(void);
    __interrupt void epwm1_isr(void);
    __interrupt void epwm2_isr(void);
    __interrupt void epwm3_isr(void);
    void update_compare(EPWM_INFO*);
    
    // Global variables used in this example
    EPWM_INFO epwm1_info;
    EPWM_INFO epwm2_info;
    EPWM_INFO epwm3_info;
    
    // Configure the period for each timer
    #define EPWM1_TIMER_TBPRD  2000  // Period register
    #define EPWM1_MAX_CMPA     1950
    #define EPWM1_MIN_CMPA       50
    #define EPWM1_MAX_CMPB     1950
    #define EPWM1_MIN_CMPB       50
    
    #define EPWM2_TIMER_TBPRD  2000  // Period register
    #define EPWM2_MAX_CMPA     1950
    #define EPWM2_MIN_CMPA       50
    #define EPWM2_MAX_CMPB     1950
    #define EPWM2_MIN_CMPB       50
    
    #define EPWM3_TIMER_TBPRD  2000  // Period register
    #define EPWM3_MAX_CMPA      950
    #define EPWM3_MIN_CMPA       50
    #define EPWM3_MAX_CMPB     1950
    #define EPWM3_MIN_CMPB     1050
    
    // To keep track of which way the compare value is moving
    #define EPWM_CMP_UP   1
    #define EPWM_CMP_DOWN 0
    
    void main(void)
    {
    // Step 1. Initialize System Control:
    // Enable Peripheral Clocks
    // This example function is found in the F28M35x_SysCtrl.c file.
        InitSysCtrl();
    
    // Step 2. Initalize GPIO:
    // This example function is found in the F28M35x_Gpio.c file and
    // illustrates how to set the GPIO to it's default state.
    // InitGpio();  // Skipped for this example
    
    // For this case just init GPIO pins for ePWM1, ePWM2, ePWM3
    // These functions are in the F28M35x_EPwm.c file
        InitEPwm1Gpio();
        InitEPwm2Gpio();
        InitEPwm3Gpio();
    
    // Step 3. Clear all interrupts and initialize PIE vector table:
    // Disable CPU interrupts
        DINT;
    
    // Initialize the PIE control registers to their default state.
    // The default state is all PIE interrupts disabled and flags
    // are cleared.
    // This function is found in the F28M35x_PieCtrl.c file.
        InitPieCtrl();
    
    // Disable CPU interrupts and clear all CPU interrupt flags:
        IER = 0x0000;
        IFR = 0x0000;
    
    // Initialize the PIE vector table with pointers to the shell Interrupt
    // Service Routines (ISR).
    // This will populate the entire table, even if the interrupt
    // is not used in this example.  This is useful for debug purposes.
    // The shell ISR routines are found in F28M35x_DefaultIsr.c.
    // This function is found in F28M35x_PieVect.c.
        InitPieVectTable();
    
    // Interrupts that are used in this example are re-mapped to
    // ISR functions found within this file.
        EALLOW; // This is needed to write to EALLOW protected registers
        PieVectTable.EPWM1_INT = &epwm1_isr;
        PieVectTable.EPWM2_INT = &epwm2_isr;
        PieVectTable.EPWM3_INT = &epwm3_isr;
        EDIS;   // This is needed to disable write to EALLOW protected registers
    
    // Step 4. Initialize all the Device Peripherals:
    // This function is found in F28M35x_InitPeripherals.c
    // InitPeripherals();  // Not required for this example
    
    // For this example, only initialize the ePWM
    
        EALLOW;
        SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0;
        EDIS;
    
        InitEPwm1Example();
        InitEPwm2Example();
        InitEPwm3Example();
    
        EALLOW;
        SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1;
        EDIS;
    
    // Step 5. User specific code, enable interrupts:
    
    // Enable CPU INT3 which is connected to EPWM1-3 INT:
        IER |= M_INT3;
    
    // Enable EPWM INTn in the PIE: Group 3 interrupt 1-3
        PieCtrlRegs.PIEIER3.bit.INTx1 = 1;
        PieCtrlRegs.PIEIER3.bit.INTx2 = 1;
        PieCtrlRegs.PIEIER3.bit.INTx3 = 1;
    
    // Enable global Interrupts and higher priority real-time debug events:
        EINT;  // Enable Global interrupt INTM
        ERTM;  // Enable Global realtime interrupt DBGM
    
    // Step 6. IDLE loop. Just sit and loop forever (optional):
        for(;;)
        {
            asm ("          NOP");
        }
    
    }
    
    __interrupt void epwm1_isr(void)
    {
        // Update the CMPA and CMPB values
        update_compare(&epwm1_info);
    
        // Clear INT flag for this timer
        EPwm1Regs.ETCLR.bit.INT = 1;
    
        // Acknowledge this interrupt to receive more interrupts from group 3
        PieCtrlRegs.PIEACK.all = PIEACK_GROUP3;
    }
    
    __interrupt void epwm2_isr(void)
    {
    
        // Update the CMPA and CMPB values
        update_compare(&epwm2_info);
    
        // Clear INT flag for this timer
        EPwm2Regs.ETCLR.bit.INT = 1;
    
        // Acknowledge this interrupt to receive more interrupts from group 3
        PieCtrlRegs.PIEACK.all = PIEACK_GROUP3;
    }
    
    __interrupt void epwm3_isr(void)
    {
    
        // Update the CMPA and CMPB values
        update_compare(&epwm3_info);
    
        // Clear INT flag for this timer
        EPwm3Regs.ETCLR.bit.INT = 1;
    
        // Acknowledge this interrupt to receive more interrupts from group 3
        PieCtrlRegs.PIEACK.all = PIEACK_GROUP3;
    }
    
    void InitEPwm1Example()
    {
    
        // Setup TBCLK
        EPwm1Regs.TBPRD = EPWM1_TIMER_TBPRD;          // Set timer period 801 TBCLKs
        EPwm1Regs.TBPHS.half.TBPHS = 0x0000;          // Phase is 0
        EPwm1Regs.TBCTR = 0x0000;                     // Clear counter
    
        // Set Compare values
        EPwm1Regs.CMPA.half.CMPA = EPWM1_MIN_CMPA;    // Set compare A value
        EPwm1Regs.CMPB = EPWM1_MAX_CMPB;              // Set Compare B value
    
        // Setup counter mode
        EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
        EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE;       // Disable phase loading
        EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;      // Clock ratio to SYSCLKOUT
        EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1;
    
        // Setup shadowing
        EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
        EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
        EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // Load on Zero
        EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
    
        // Set actions
        EPwm1Regs.AQCTLA.bit.CAU = AQ_SET;            // Set PWM1A on event A, up
                                                      // count
        EPwm1Regs.AQCTLA.bit.CAD = AQ_CLEAR;          // Clear PWM1A on event A,
                                                      // down count
    
        EPwm1Regs.AQCTLB.bit.CBU = AQ_SET;            // Set PWM1B on event B, up
                                                      // count
        EPwm1Regs.AQCTLB.bit.CBD = AQ_CLEAR;          // Clear PWM1B on event B,
                                                      // down count
    
        // Interrupt where we will change the Compare Values
        EPwm1Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO;     // Select INT on Zero event
        EPwm1Regs.ETSEL.bit.INTEN = 1;                // Enable INT
        EPwm1Regs.ETPS.bit.INTPRD = ET_3RD;           // Generate INT on 3rd event
    
        // Information this example uses to keep track
        // of the direction the CMPA/CMPB values are
        // moving, the min and max allowed values and
        // a pointer to the correct ePWM registers
        epwm1_info.EPwm_CMPA_Direction = EPWM_CMP_UP;  // Start by increasing CMPA &
        epwm1_info.EPwm_CMPB_Direction = EPWM_CMP_DOWN; // decreasing CMPB
        epwm1_info.EPwmTimerIntCount = 0;              // Zero the interrupt counter
        epwm1_info.EPwmRegHandle = &EPwm1Regs;         // Set the pointer to the
                                                       // ePWM module
        epwm1_info.EPwmMaxCMPA = EPWM1_MAX_CMPA;       // Setup min/max CMPA/CMPB
                                                       // values
        epwm1_info.EPwmMinCMPA = EPWM1_MIN_CMPA;
        epwm1_info.EPwmMaxCMPB = EPWM1_MAX_CMPB;
        epwm1_info.EPwmMinCMPB = EPWM1_MIN_CMPB;
    
    }
    
    void InitEPwm2Example()
    {
    
        // Setup TBCLK
        EPwm2Regs.TBPRD = EPWM2_TIMER_TBPRD;          // Set timer period 801 TBCLKs
        EPwm2Regs.TBPHS.half.TBPHS = 0x0000;          // Phase is 0
        EPwm2Regs.TBCTR = 0x0000;                     // Clear counter
    
        // Set Compare values
        EPwm2Regs.CMPA.half.CMPA = EPWM2_MIN_CMPA;    // Set compare A value
        EPwm2Regs.CMPB = EPWM2_MIN_CMPB;              // Set Compare B value
    
        // Setup counter mode
        EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
        EPwm2Regs.TBCTL.bit.PHSEN = TB_DISABLE;       // Disable phase loading
        EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;      // Clock ratio to SYSCLKOUT
        EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV1;
    
        // Setup shadowing
        EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
        EPwm2Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
        EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // Load on Zero
        EPwm2Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
    
        // Set actions
        EPwm2Regs.AQCTLA.bit.CAU = AQ_SET;           // Set PWM2A on event A, up
                                                     // count
        EPwm2Regs.AQCTLA.bit.CBD = AQ_CLEAR;         // Clear PWM2A on event B, down
                                                     // count
    
        EPwm2Regs.AQCTLB.bit.ZRO = AQ_CLEAR;         // Clear PWM2B on zero
        EPwm2Regs.AQCTLB.bit.PRD = AQ_SET  ;         // Set PWM2B on period
    
        // Interrupt where we will change the Compare Values
        EPwm2Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO;    // Select INT on Zero event
        EPwm2Regs.ETSEL.bit.INTEN = 1;               // Enable INT
        EPwm2Regs.ETPS.bit.INTPRD = ET_3RD;          // Generate INT on 3rd event
    
        // Information this example uses to keep track
        // of the direction the CMPA/CMPB values are
        // moving, the min and max allowed values and
        // a pointer to the correct ePWM registers
        epwm2_info.EPwm_CMPA_Direction = EPWM_CMP_UP;  // Start by increasing CMPA &
        epwm2_info.EPwm_CMPB_Direction = EPWM_CMP_UP;  // increasing CMPB
        epwm2_info.EPwmTimerIntCount = 0;              // Zero the interrupt counter
        epwm2_info.EPwmRegHandle = &EPwm2Regs;         // Set the pointer to the
                                                       // ePWM module
        epwm2_info.EPwmMaxCMPA = EPWM2_MAX_CMPA;       // Setup min/max CMPA/CMPB
                                                       // values
        epwm2_info.EPwmMinCMPA = EPWM2_MIN_CMPA;
        epwm2_info.EPwmMaxCMPB = EPWM2_MAX_CMPB;
        epwm2_info.EPwmMinCMPB = EPWM2_MIN_CMPB;
    
    }
    
    void InitEPwm3Example(void)
    {
    
        // Setup TBCLK
        EPwm3Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up/down
        EPwm3Regs.TBPRD = EPWM3_TIMER_TBPRD;         // Set timer period
        EPwm3Regs.TBCTL.bit.PHSEN = TB_DISABLE;      // Disable phase loading
        EPwm3Regs.TBPHS.half.TBPHS = 0x0000;         // Phase is 0
        EPwm3Regs.TBCTR = 0x0000;                    // Clear counter
        EPwm3Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;     // Clock ratio to SYSCLKOUT
        EPwm3Regs.TBCTL.bit.CLKDIV = TB_DIV1;
    
        // Setup shadow register load on ZERO
        EPwm3Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
        EPwm3Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
        EPwm3Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
        EPwm3Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
    
        // Set Compare values
        EPwm3Regs.CMPA.half.CMPA = EPWM3_MIN_CMPA;   // Set compare A value
        EPwm3Regs.CMPB = EPWM3_MAX_CMPB;             // Set Compare B value
    
        // Set Actions
        EPwm3Regs.AQCTLA.bit.PRD = AQ_SET;           // Set PWM3A on period
        EPwm3Regs.AQCTLA.bit.CBD = AQ_CLEAR;         // Clear PWM3A on event B, down
                                                     // count
    
        EPwm3Regs.AQCTLB.bit.PRD = AQ_CLEAR;         // Clear PWM3A on period
        EPwm3Regs.AQCTLB.bit.CAU = AQ_SET;           // Set PWM3A on event A, up
                                                     // count
    
        // Interrupt where we will change the Compare Values
        EPwm3Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO;    // Select INT on Zero event
        EPwm3Regs.ETSEL.bit.INTEN = 1;               // Enable INT
        EPwm3Regs.ETPS.bit.INTPRD = ET_3RD;          // Generate INT on 3rd event
    
        // Information this example uses to keep track
        // of the direction the CMPA/CMPB values are
        // moving, the min and max allowed values and
        // a pointer to the correct ePWM registers
        epwm3_info.EPwm_CMPA_Direction = EPWM_CMP_UP;  // Start by increasing CMPA &
        epwm3_info.EPwm_CMPB_Direction = EPWM_CMP_DOWN; // decreasing CMPB
        epwm3_info.EPwmTimerIntCount = 0;              // Zero the interrupt counter
        epwm3_info.EPwmRegHandle = &EPwm3Regs;         // Set the pointer to the
                                                       // ePWM module
        epwm3_info.EPwmMaxCMPA = EPWM3_MAX_CMPA;       // Setup min/max CMPA/CMPB
                                                       // values
        epwm3_info.EPwmMinCMPA = EPWM3_MIN_CMPA;
        epwm3_info.EPwmMaxCMPB = EPWM3_MAX_CMPB;
        epwm3_info.EPwmMinCMPB = EPWM3_MIN_CMPB;
    
    }
    
    void update_compare(EPWM_INFO *epwm_info)
    {
    
        // Every 10'th interrupt, change the CMPA/CMPB values
        if(epwm_info->EPwmTimerIntCount == 10)
        {
            epwm_info->EPwmTimerIntCount = 0;
    
            // If we were increasing CMPA, check to see if
            // we reached the max value.  If not, increase CMPA
            // else, change directions and decrease CMPA
            if(epwm_info->EPwm_CMPA_Direction == EPWM_CMP_UP)
            {
                if(epwm_info->EPwmRegHandle->CMPA.half.CMPA <
                   epwm_info->EPwmMaxCMPA)
                {
                    epwm_info->EPwmRegHandle->CMPA.half.CMPA++;
                }
                else
                {
                    epwm_info->EPwm_CMPA_Direction = EPWM_CMP_DOWN;
                    epwm_info->EPwmRegHandle->CMPA.half.CMPA--;
                }
            }
    
            // If we were decreasing CMPA, check to see if
            // we reached the min value.  If not, decrease CMPA
            // else, change directions and increase CMPA
            else
            {
                if(epwm_info->EPwmRegHandle->CMPA.half.CMPA ==
                   epwm_info->EPwmMinCMPA)
                {
                    epwm_info->EPwm_CMPA_Direction = EPWM_CMP_UP;
                    epwm_info->EPwmRegHandle->CMPA.half.CMPA++;
                }
                else
                {
                    epwm_info->EPwmRegHandle->CMPA.half.CMPA--;
                }
            }
    
            // If we were increasing CMPB, check to see if
            // we reached the max value.  If not, increase CMPB
            // else, change directions and decrease CMPB
            if(epwm_info->EPwm_CMPB_Direction == EPWM_CMP_UP)
            {
                if(epwm_info->EPwmRegHandle->CMPB < epwm_info->EPwmMaxCMPB)
                {
                    epwm_info->EPwmRegHandle->CMPB++;
                }
                else
                {
                    epwm_info->EPwm_CMPB_Direction = EPWM_CMP_DOWN;
                    epwm_info->EPwmRegHandle->CMPB--;
                }
            }
    
            // If we were decreasing CMPB, check to see if
            // we reached the min value.  If not, decrease CMPB
            // else, change directions and increase CMPB
    
            else
            {
                if(epwm_info->EPwmRegHandle->CMPB == epwm_info->EPwmMinCMPB)
                {
                    epwm_info->EPwm_CMPB_Direction = EPWM_CMP_UP;
                    epwm_info->EPwmRegHandle->CMPB++;
                }
                else
                {
                    epwm_info->EPwmRegHandle->CMPB--;
                }
            }
        }
        else
        {
            epwm_info->EPwmTimerIntCount++;
        }
    
        return;
    }
    
    
    
    

    Regards,

    Gautam

  • I've done with PWM without any interrupts, ADC etc. Problem was in the working with two core in the debug mode. I still don't good understand how launch debug with two core. But simplest PWM is working. Gautam, thank you very much for your attendance and advice.

    Regards.

  • That's great. For debugging 2 cores check this out:

    http://e2e.ti.com/support/microcontrollers/c2000/f/171/t/166587.aspx

    Good luck, Merry Christmas & Regards,

    Gautam