Hello,
I am looking at the code for the TMDSHVRESLLCKIT. There are four ADC signals that are sampled:
ADC-A2 => I-SR1/V-SR1/COMP1
ADC-A4 => I-SR2/V-SR2/COMP2
ADC-A7 => Vo-fb
ADC-B1 => Ipri-cs
These channels get set up in the following array:
// ADC Channel Selection
ChSel[0] = 9; // Dummy read for first sample bug
ChSel[1] = 9; // B1 - Ipri
ChSel[2] = 2; // A2 - V_SR1 / I_SR1
ChSel[3] = 2; // A2 - V_SR1 / I_SR1
ChSel[4] = 4; // A4 - V_SR2 / I_SR2
ChSel[5] = 4; // A4 - V_SR2 / I_SR2
ChSel[6] = 7; // A7 - Vout
ChSel[7] = 7; // A7 - Vout
then are passed into the following function:
ADC_SOC_CNF(ChSel, TrigSel, ACQPS, 17, 0);
My question is in regard to some #defines that are used by the kit's GUI:
#define IpriR AdcResult.ADCRESULT1 //Q12
#define V_SR1R AdcResult.ADCRESULT3 //Q12
#define V_SR2R AdcResult.ADCRESULT5 //Q12
#define I_SR1R AdcResult.ADCRESULT3 //Q12
#define I_SR2R AdcResult.ADCRESULT5 //Q12
#define VoutR AdcResult.ADCRESULT7 //Q12
I can see how ADC-A7 maps to AdcResult.ADCRESULT7.
I am not sure how ADC-A2 maps to AdcResult.ADCRESULT3?
I am not sure how ADC-A4 maps to AdcResult.ADCRESULT5?
They are off by one??
I am not sure how ADC-B1 maps to AdcResult.ADCRESULT1? I would think it would be AdcResult.ADCRESULT9?
Any clarification would be great.
Thanks,
Brent