Other Parts Discussed in Thread: DRV8301, MOTORWARE
Hi all,
I'm in a dilly of a pickle - I just finished populating my 'proper' board (based on a prototype I posted here for anyone that remembers) and, no surprises, it didn't work. The problem is TZ2 is tripped:
There is no fault - in fact, I can watch GPIO28 go from high to low when I deliberately set the supply voltage to <5.5V. So that all seems to be working and OCTW is also not reporting a fault. Both GPIO28&29 are high.
Interestingly, I can turn the PWMs on by manually turning off en_gate - by that I mean toggling the register... At this point TZ2 flag remains high but I can now clear it (manually setting the bit in clear register)... When I turn en_gate back on, TZ2 latches again... turning off the PWMs.
Half my ADC results are 0x00, (the bottom half) pretty sure this is not the cause, but the result of the problem as they are the phase currents?
So, what, besides OCTW and FAULT (GPIO 29/28), can cause TZ2 to trip on the BOOSTDRV8301?
Thanks