Other Parts Discussed in Thread: DRV8312, MOTORWARE
Hi there
I've got a bit of an issue here. I use the DRV8312 Kit with a F2803x controlCARD which works very well. For a new project, I have to switch to a F2806x ISO controlCARD, which gets rather hot when I plug it into the DIMM socket. In addition to that, I cannot run the GUI-Project delivered with the DRV Kit on the F2806x card. It works on the F2803x module though.
Is there any kind of limitation or am I just doing it wrong?
Regards,
Patrick