We would like to utilize the HRPWM output from something like a TMS320F2802x (e.g. LaunchPad XL) to generate a sine wave. The output of the PWM will be complementary drive signals connected to a half bridge driver. I was hoping to use the dead-band submodule in the DSP, however, it appears that will not work if the PWMA output is fed through the HRPWM section.
Our options as I understand it are:
1. Use an additional PWMA channel with HRPWM but configured with the opposite polarity and adjust the CMPA thresholds to achieve dead-band protection
2. Use a half-bridge driver with built-in shoot-through protection
Did I miss anything?
Thanks,
John