Other Parts Discussed in Thread: MOTORWARE, DRV8301
Hello,
Sorry to bother you with a new question.
I have spent time trying to identify a three-phase asynchronous motor with InstaSPIN-MOTION, DRV8301-HC-EVM and F28069 ISO controlCARD.
Every time a same critical error occurs on the GUI like this:
So I can’t start my project. I wonder if there is something wrong with my parameters of Identification Settings and Control Timing ? Could you give me some advice ?
Motor parameters:
Model: ZPJ0.75-90S-4
Rated Power: 750W
Rated frequency: 90Hz
Rated voltage: 16V
Rated current: 43A
Rated speed: 2600r/min
Rated torque: 2.5N.m
Thanks very much,
Brant Zheng.