Other Parts Discussed in Thread: DRV8301, MOTORWARE
Hi,
Recently purchased the DRV8301 with 28069 control card. I was running lab4 of InstaSPIN and PMSM motor was spinning with 48V and under no load condition i.e., <0.5 amp. While I was attempting to rerun the Fault LED was active. Tried all means and reinstalled motorware too. It did not help to sort. Tried to reduce the voltage PVDD to 12V and the Fault LED is active the moment the program is run.
Checked the SPI 8301 registers it shows FAULT-1024 & GCDD_UV 512.
Let me know how to sort this.
thx