This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Everyone,
I recently received a new Concerto Development tool (F28M36 P63C2 daughter card+Docking station) and I was very exited to test it. I installed the Code Composer Studio Version: 6.0.1.00040 and I imported ADC SOC C28X example file from F28M36X "code examples" folder.
First of all, why should it be so difficult to run an example file? it took me a couple of hours to get my head around the example code and how to get rid of 7 errors that it was giving me. turns out that I had two cmd files one in common folder and on in the example project.
Anyways, I can now build the imported project. I have green ticks for Step 1 and 2! for Step 3 after a few hiccups I could select the XDS100V2 which I believe the correct inbuilt debugging tool. so that is fine as well.
Step 4 Debug the imported project I am receiving this error:
Error connecting to the target:
(Error -2131 @ 0x0)
Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 5.1.507.0)
I have not done any changes to the board so everything is factory default.
Am I missing anything there?
I appreciate your comments
Hi Everyone,
Keep cool, I was missing power!!!
There was no power supply in the box and only one USB cable so I assumed it is the only cable I need.
Well now with two USB cables one to the docking station (power supply) and one to the control board (communications) it is working fine!
Cheers,
Hi Mohsen,
Mohsen Mesbah said:First of all, why should it be so difficult to run an example file? it took me a couple of hours to get my head around the example code and how to get rid of 7 errors that it was giving me. turns out that I had two cmd files one in common folder and on in the example project.
You should've gone through the workshop/training session first for quick understanding of the structure and methodology. You can find the same here:
http://www.ti.com/mcu/docs/mcuorphan.tsp?contentId=129766
Regards,
Gautam