Other Parts Discussed in Thread: AFE031
Hi
I'am using TMS320C2000 Developer's Kit. I've imported in CCSv6 a G3 PHY Test example and i've modified it. When I build the project the following errors occur:
undefined first referenced
>> Compilation failure
symbol in file
--------- ----------------
_PHY_rxPpduStart ./main.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "g328069_1.out" not built
gmake: *** [g328069_1.out] Error 1
gmake: Target `all' not remade because of errors.
I think the error is caused by the absence of a declaration in a library, specifically "phy_vcu_afe031.lib". Infact in the header file phy_rx.h there are the following function prototypes:
PHY_status_t PHY_rxInit(void);
PHY_status_t PHY_rxStart(UINT16 timeOut, PHY_cbFunc_t cb_p);
PHY_status_t PHY_rxSuspend(PHY_cbFunc_t cb_p);
PHY_status_t PHY_rxResume(void);
PHY_status_t PHY_rxPpduStart(PHY_cbFunc_t cb_p);
PHY_status_t PHY_rxPpduStop(void);
PHY_status_t PHY_rxPpduRelease(PHY_rxPpdu_t *ppdu_p);
PHY_status_t PHY_rxSet(UINT16 setType, PHY_rxSetData_t *setData_p);
PHY_status_t PHY_rxGet(UINT16 getType, PHY_rxGetData_t *getData_p);
PHY_status_t PHY_rxGetStat(PHY_rx_stat_t *getData_p);
PHY_status_t PHY_rxSmRun(PHY_rxProc_t procType);
PHY_status_t PHY_rxBitStartIndicate(PHY_cbFunc_t cb_p);
PHY_status_t PHY_rxPhyTimingIndicate(PHY_cbFunc_t cb_p);
I can find in phy_vcu_afe031.lib lines like this:
PHY_rxInit T:/csa_group_emeter/dspsrdc_csa/emeter/dsp_c28x/G3/src/phy/rx/phy_rx_main.c ... and other symbols that i can't decode in a text file.
And so for each function listed in phy_rx.h, except for PHY_rxPpduStart(), and this remind the symbol involved in error #10234-D.
Could anyone help me to fix this problem or tell me where i can find a library that includes PHY_rx_PpduStart?
Regards.