Hi, Everyone.
I am working on a project which used F28035. When it works with full load, the chip would reset.
The VDDIO and VDDA is OK, and the XRS pin is fine.
1. How many reset sources does the F28035 have?
2. If the voltagge of the gpio or ad channel is out of range, the chip may reset?