Other Parts Discussed in Thread: TMS320F28335, CONTROLSUITE
Dear All,
I am using Code Composer Studio v6.0 for developing embedded application on TMS320F28335 platform.
I am using CpuTimer0 to schedule an event. Inside CpuTimer0 ISR, i am setting a flag immediately after entering ISR. This flag is detected in while(1) super-loop for further processing. Flag doesn't sets immediately after entering ISR and hence processing doesn't starts after entering while(1) super-loop.
However, if a add a delay of one instruction cycle immediately after entering ISR and before setting flag, the flag is detected in while(1) super-loop and further processing starts.
Why is the delay required immediately after entering ISR and before setting the flag, so that the flag can be detected correctly in while(1) super-loop ?
I have pasted the code below.
Thank you,
Sunil Sawant
/*----------------------- ISR code without delay - Start ------------------------- */
// INT1.7
interrupt void TINT0_ISR(void) // CPU-Timer 0
{
// Insert ISR Code here
tTMS320F2812ECanaTransactionStatusFlags.TransactionCycle.bit.b1CanTxnCycleStart = TRUE;
// Clear Timer0 interrupt flag
CpuTimer0Regs.TCR.bit.TIF = 1;
// To receive more interrupts from this PIE group, acknowledge this interrupt
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
IER |= M_INT1; // Enable INT1
EINT;
return;
// Next two lines for debug only to halt the processor here
// Remove after inserting ISR Code
//asm (" ESTOP0");
//for(;;);
}
/*----------------------- ISR code without delay - End ------------------------- */
/*----------------------- ISR code with delay - Start ------------------------- */
// INT1.7
interrupt void TINT0_ISR(void) // CPU-Timer 0
{
// Insert ISR Code here
// This is delay
GpioDataRegs.GPBTOGGLE.bit.GPIOB0 = 1;
tTMS320F2812ECanaTransactionStatusFlags.TransactionCycle.bit.b1CanTxnCycleStart = TRUE;
// Clear Timer0 interrupt flag
CpuTimer0Regs.TCR.bit.TIF = 1;
// To receive more interrupts from this PIE group, acknowledge this interrupt
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
IER |= M_INT1; // Enable INT1
EINT;
return;
// Next two lines for debug only to halt the processor here
// Remove after inserting ISR Code
//asm (" ESTOP0");
//for(;;);
}
/*----------------------- ISR code with delay - End ------------------------- */