Other Parts Discussed in Thread: TMS320F28377D, CONTROLSUITE
Hey,
Anyone how can help me? I am struggling with a TMS320F28377D, rev B, McBSP transmits, controlled by DMA:
The idea is to send "Buffer" from RAM via DMA to McBSP DX. The buffer is filled with non-zero data.
I followed the example from the controlsuite, studied the manual for both DMA and McBSP.
But the output I see on my scope only shows 0x0000 and not the expected data.
Here's my code:
#define DataSize 300
Uint32 Buffer[DataSize+1];
void mcbsp_init()
{
EALLOW;
CpuSysRegs.PCLKCR11.bit.McBSP_A = 1; // enable McBSP-A peripheral
EDIS;
udelay(1);
McbspaRegs.SPCR2.all = 0x0000; // Reset FS generator, sample rate generator & transmitter.
McbspaRegs.SPCR1.all = 0x0000; // Reset Receiver, Right justify word
udelay(1);
McbspaRegs.SPCR2.bit.FREE = 1;
McbspaRegs.SPCR2.bit.SOFT = 1;
McbspaRegs.MFFINT.all = 0x0; // Disable all interrupts
McbspaRegs.MFFINT.bit.XINT = 1;
McbspaRegs.SPCR2.bit.XINTM = 2; // on every FSX
udelay(1);
McbspaRegs.RCR2.all = 0x0; // Single-phase frame, 1 word/frame, No companding
McbspaRegs.RCR1.all = 0x0;
udelay(1);
McbspaRegs.XCR1.all = 0x0040; // frame length = 1 word, word length = 16 bit
McbspaRegs.XCR2.all = 0x0240;
udelay(1);
McbspaRegs.SRGR2.bit.CLKSM = 1; // SCLKME=0, so clock to SRG is LSPCLK
McbspaRegs.SRGR2.bit.FPER = 20; // FPER = 20 CLKG periods
McbspaRegs.SRGR2.bit.FSGM = 1;
udelay(1);
McbspaRegs.SRGR1.bit.FWID = 15; // Frame Width = 16 CLKG period
McbspaRegs.SRGR1.bit.CLKGDV = 255; // CLKG frequency = LSPCLK/(CLKGDV+1) = 14.28M/256 = 55.8KHz
udelay(1);
McbspaRegs.PCR.bit.FSXM = 1; // FSX generated internally
McbspaRegs.PCR.bit.CLKXM = 1; // CLKX generated internally
udelay(1);
McbspaRegs.SPCR2.bit.GRST = 1; // Enable the sample rate generator
udelay(1);
McbspaRegs.SPCR2.bit.FRST = 1; // Frame Sync Generator enabled
udelay(1);
return;
}
void dma_init(void)
{
// configure DMA:
EALLOW;
CpuSysRegs.PCLKCR0.bit.DMA = 1;
udelay(10);
DmaRegs.DMACTRL.bit.HARDRESET = 1;
udelay(10);
// Channel 1, McBSPA transmit only
DmaRegs.CH1.MODE.bit.CHINTE = 0; // no interrupts to CPU
DmaRegs.CH1.BURST_SIZE.all = 0; // 1 word/burst
DmaRegs.CH1.SRC_BURST_STEP = 0; // no effect when using 1 word/burst
DmaRegs.CH1.DST_BURST_STEP = 0; // no effect when using 1 word/burst
DmaRegs.CH1.TRANSFER_SIZE = DataSize; // number of transfers
DmaRegs.CH1.SRC_TRANSFER_STEP = 1; // Move to next word (move address pointer 2 bytes)
DmaRegs.CH1.DST_TRANSFER_STEP = 0; // Don't move destination address
DmaRegs.CH1.SRC_ADDR_SHADOW = (Uint32 )&Buffer[0]; // Start address = buffer
DmaRegs.CH1.DST_ADDR_SHADOW = (Uint32) &McbspaRegs.DXR1.all; // Start address = McBSPA DXR
DmaRegs.CH1.CONTROL.bit.PERINTCLR = 1; // Clear peripheral interrupt event flag
DmaRegs.CH1.CONTROL.bit.SYNCCLR = 1; // Clear sync flag
DmaRegs.CH1.CONTROL.bit.ERRCLR = 1; // Clear sync error flag
DmaRegs.CH1.DST_WRAP_SIZE = DmaRegs.CH1.TRANSFER_SIZE + 10; // disable wrapping by setting wrap_size higher than Transfer_Size.
DmaRegs.CH1.SRC_WRAP_SIZE = DmaRegs.CH1.TRANSFER_SIZE + 10; // disable wrapping by setting wrap_size higher than Transfer_Size.
DmaRegs.CH1.MODE.bit.SYNCE = 0; // No sync signal
DmaRegs.CH1.MODE.bit.SYNCSEL = 0; // No sync signal
DmaRegs.CH1.MODE.bit.ONESHOT = 1; // multiple sends per transfer.
DmaRegs.CH1.MODE.bit.CONTINUOUS = 1; // keep on going during debug
DmaRegs.CH1.MODE.bit.PERINTE = 1; // Enable peripheral interrupt event
DmaRegs.CH1.MODE.bit.PERINTSEL = 1; // simply CH1. old-> //DMA_MXEVTA; // Peripheral interrupt select = McBSP MXSYNCA
DmaClaSrcSelRegs.DMACHSRCSEL1.bit.CH1 = DMA_MXEVTA;
DmaRegs.DEBUGCTRL.bit.FREE = 1;
DmaRegs.CH1.CONTROL.bit.PERINTCLR = 1;
udelay(1);
EDIS;
udelay(1);
return;
}
void main(void)
{
int i;
EALLOW;
IER = 0x0000;
IFR = 0x0000;
DINT;
EDIS;
InitSysCtrl();
for (i=0;i<DataSize;i++) Buffer[i] =( (Uint32)(0x1201+i)<<16)+(0xF0F0-i); // generate non-zero sort-of recognizable data.
EALLOW;
ClkCfgRegs.LOSPCP.bit.LSPCLKDIV = 7; // 200MHz/14 = 14.28MHz
EDIS;
// configure pins for McBSP peripheral:
EALLOW;
GpioCtrlRegs.GPCMUX2.bit.GPIO84 = 3;
GpioCtrlRegs.GPCMUX2.bit.GPIO85 = 3;
GpioCtrlRegs.GPCMUX2.bit.GPIO86 = 3;
GpioCtrlRegs.GPCMUX2.bit.GPIO87 = 3;
GpioCtrlRegs.GPCGMUX2.bit.GPIO84 = 3;
GpioCtrlRegs.GPCGMUX2.bit.GPIO85 = 3;
GpioCtrlRegs.GPCGMUX2.bit.GPIO86 = 3;
GpioCtrlRegs.GPCGMUX2.bit.GPIO87 = 3;
EDIS;
dma_init();
// Start DMA:
EALLOW;
DmaRegs.CH1.CONTROL.bit.RUN = 1; // Start DMA Transmit from McBSP-A
EDIS;
udelay(1);
// Configure McBSP
mcbsp_init();
udelay(1);
// start McBSP:
McbspaRegs.SPCR2.bit.XRST=1; // Release TX from Reset
for (;;)
{
// check scope.
}
}