Part Number: TMS320F28377D
Other Parts Discussed in Thread: TMS320C6657,
Hi.
I try to communicate through McBSP in DMA mode between a TMS320F28377D (DELFINO) and a TMS320C6657 (C66).
I can't use McBSP as SPI because the C66 processsor doesn't support SPI protocol (see document SPRUHH0—May 2012 paragraph 2.10).
So I'd like to have the same configuration for C66 and DELFINO processors.
Below, I'd like to give you an example what I want (for simplify the graph, I represent a transfer with 2 words of 8 bits instead of two words of 16 bits) :
With my current configuration, I have a frame synchronisation signal between each word.
Do you have any idea of register configuration that allows to have the operating mode in the graph ?
Thanks in advance.