I have a low inductance high speed motor. (Link: http://www.nmbtc.com/motors/part-numbers/Brushless-DC-25mm/BLDC24P16A-06V/6462
I'm able to get it to detect and spin in lab02c. When re-enabling identify_run after the identification steps, in runs fairly stable. I'm able to adjust the speed between 500 RPM and ~8000 RPM, and have verified with a flashlamp that gMotorVars.Speed_krpm is reporting correctly. The identification reports Rs=0.172515, and Ls=11.86E-6. My motor parameters appear as follows:
#elif (USER_MOTOR == PMDM_BLDC24P16A)
#define USER_MOTOR_TYPE MOTOR_Type_Pm
#define USER_MOTOR_NUM_POLE_PAIRS (3)
#define USER_MOTOR_Rr (NULL)
#define USER_MOTOR_Rs (0.172515)
#define USER_MOTOR_Ls_d (1.186E-5)
#define USER_MOTOR_Ls_q (1.186E-5)
#define USER_MOTOR_RATED_FLUX (NULL)
#define USER_MOTOR_MAGNETIZING_CURRENT (NULL)
#define USER_MOTOR_RES_EST_CURRENT (1.0)
#define USER_MOTOR_IND_EST_CURRENT (-1.0)
#define USER_MOTOR_MAX_CURRENT (4.8)
#define USER_MOTOR_FLUX_EST_FREQ_Hz (40.0)
When I run lab03a with the above user parameters, the motor chatters and rotates at an extremely slow speed (usually less than 20 RPM.) The user setting gMotorVars.SpeedRef_krpm does not have any effect. Additionally, gMotorVars.Speed_krpm reports wildly changing values of speed between -2000 RPM and +2000 RPM.
When running lab04 (torque controller), I'm able to get the motor turning mostly smoothly, but gMotorVars.Speed_krpm reports incorrect values. With gMotorVars.IqRef_A=1.0, the flashlamp measured speed of the motor is ~1000 RPM, but gMotorVars.Speed_krpm varies between 8640 RPM and 8790 RPM. Additionally, the motor loses control with IqRef values much past 1.0.
Questions:
* What would cause incorrect speed reporting?
* Why does speed reporting work in lab02c, but not in others?
* If lab02c detects an Ls value that slightly disagrees with my meter measured value (Eg, 1.18E-5 vs measured 1.63E-5), should I use my measured value, or lab02c's detected value?
* Should the measured value of Ls be varying with PWM frequency? I observe the following:
60 KHz: Ls=0.479E-5
70 KHz: Ls=1.02E-5
80 KHz: Ls=1.30E-5
90 KHz: Ls=2.65E-5
Thanks,
Grant