This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM320F28335 and XINTF: approximately 1/2 volt 150MHz sawtooth waveform riding on XINTF write strobe line

Guru 20035 points

I am debugging an issue where the XINTF write strobe line doesn't go low during a write.  I am using the Example_2833xDMA_xintf_to_ram example in control suite.  

I noticed that after I execute the XintfRegs.XINTCNF2.bit.CLKMODE = 0; line in init_zone7(), an approximately 1/2V 150MHz sawtooth waveform appears on the write strobe line.  I haven't taken the time to notice if this waveform is also appearing on the other XINTF lines.

Below are oscilloscope snapshots showing before and after executing the XintfRegs.XINTCNF2.bit.CLKMODE = 0; line.

What would be the reason for the waveform appearing on the write strobe line?

Update: this waveform is also appearing on the other XINTF lines.

Stephen